cancel
Showing results for 
Search instead for 
Did you mean: 

help httpserver on nucleo board: I pay for it

dieter 123
Associate III
Posted on November 22, 2017 at 10:23

Hi

I am late in y project and need some help with a HTTP server.

This is what I need:

a webserver for FW download which also gives me the opportunity to change IP Address and Netmask, ideal on a nucleo stmf429zi board, but any other would do as well.

One of the ST example projects should be taken as starting point, like this one:

STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP

A teamviewer session should be

Deliverables: 

- firmware project : WEbserver IAP to upload FW , set netmask, IP address , IPV4

- Git repository with 2 commits: example code of ST + all changes

- an application FW which just blinks some leds

- 1 hour team viewer session demo about what needed to be changed and why.

Any one interested? send me a PM

Thx

#stm32-iap
1 REPLY 1
AvaTar
Lead
Posted on November 22, 2017 at 10:44

I am already fully occupied with my own job and projects ...

Just want to paraphrase Frederick P. Brooks from his book 'The Mythical Man-Month':

'Adding more developers to a delayed project will delay it even further.'