cancel
Showing results for 
Search instead for 
Did you mean: 

HELLO! STM32L051R8T6 it has a problem with the initialization of the LSE / LSI clock?

锋赵.1
Associate

After the analysis, we know that the processor in the system is powered by a battery voltage of 3.6 V and cyclically/after meeting certain conditions, it goes into Standby mode. It is woken up by the wakeup pin. After waking up, the processor correctly enters the normal operating mode, but it has a problem with the initialization of the LSE / LSI clock, which makes it impossible to continue the program - the program hangs.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @锋 赵​, to the community!

Well, apart from a description of the problem, the photo and the value of the supply voltage, you have not provided any information such as the layout of the LSE, possibly HSE or the relevant programme section (initialisation, wake-up etc), so it is unlikely that anyone can make a statement about the cause.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.