2021-06-30 11:23 PM
2021-07-01 01:07 AM
Hello @DLev.1 and welcome to the Community 🙂
Yes, possible to use STM32L152RET6 as it's full compatible with STM32L151RET6.
If your question is answered, please close this topic by choosing Select as Best.
This will help other community members finding that answer faster.😉
Imen
2021-07-01 01:07 AM
Hello @DLev.1 and welcome to the Community 🙂
Yes, possible to use STM32L152RET6 as it's full compatible with STM32L151RET6.
If your question is answered, please close this topic by choosing Select as Best.
This will help other community members finding that answer faster.😉
Imen
2021-07-01 01:11 AM
Thank you, Imen!
2021-12-08 03:35 AM
if the two are absolute the same, why do you have both? i dont belive that, there must have some differente.... to star with, in the product selector it says 151 have dual boot and 152 not.