cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I´m not able to uncompress this file: File: en.stm32-mat_target.zip Filesize: 19.047.669 Bytes Installation File: STM32MatTarget_4.4.2_setup.exe What´s wrong with me or the file? Cheers Udo

UJuer
Associate
 
5 REPLIES 5
JWest.17
Associate II

I'm having the same issue. Did you find a work around?

Test the integrity of the file, check that you don't have AV software interfering with the un-packaging.

Download works fine here, look for issues at your end.

MD5 : 84bd587e84a62c1d518ae85fccbb0151 stm32-mat_target_v4.4.2.zip

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
UJuer
Associate

I used 7-Zip and it worked.

Using WinRAR here, integrity test passes, file unpacks and executes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Cyril FENARD
ST Employee

Hi @Community member​ ,

The version 5.1.0 of STM32-MAT/TARGET has just published end of July 2019.

The packing and installation have been revisited in this version.

Hoping that your installation is easier now.

Regards.

Cyril