2017-04-11 6:07 AM
Hello guys, plzz does someone use ADC multichannel, i tried and i use 2 temperatur sensors but they dont give same or approximate values ?!?
2017-04-11 6:30 AM
Hi
rachidi.yousra
,There is many ADC examples within STM32Cube firmware package, I would recommend you the ready-use example in the cube package relevant to the device that you are using to understand the principle.
For more clarification your may refer to your reference manual and this
STM32™’s ADC modes and their applications.Imen
2017-04-11 7:18 AM
thanks Imen, i will see the manual
2017-04-11 8:07 AM
There are hundreds of STM32 parts at this point, you need to be specific about what model/family you are using.
It is also helpful to provide the code that isn't working, it is hard to review things that can't be seen.
2017-04-11 5:42 PM