2008-09-25 6:57 PM
header files revisited
2011-05-17 3:45 AM
Quote:
I'm pleased to announce you that we have released a new FW Library version 2.0.3 that adds and extends support for header files where a description of all registers and bit definitions are provided in a file called ''stm32f10x_map.h''.Thanks, this is really excellent news. I downloaded the new fwlib, and went to my code where I had created a duplicate definition of CAN_TSR_TME0 (for example). Looking through the fwlib, I see in stm32f10x_map.h: #define CAN_TSR_TME0 ((u32)0x04000000) /* Transmit Mailbox 0 Empty */ In stm32f10x_can.c, I see this: #define TSR_TME0 ((u32)0x04000000) /* Transmit mailbox 0 empty */ stm32f10x_can.c includes stm32f10x_can.h, which includes stm32f10x_map.h. So the definition of CAN_TSR_TME0 from stm32f10x_map.h is available to stm32f10x_can.c, and yet, instead of simply removing CAN_TSR_TME0 from stm32f10x_can.c and using the definition from the header, instead someone renamed the definition in the .c to TSR_TME0, perhaps to avoid a conflict with the other #define. There's obviously many reasons why that's a bad idea: 1) Duplicate definitions need to be maintained in parallel 2) Only the definition in stm32f10x_can.c is being tested by ST's fwlib example programs, so if the one in _map.h is wrong, it won't be noticed by anyone running the example apps. 3) Because stm32f10x_can.c has it's own definitions, a working example app won't tell you that everything necessary is in stm32f10x_map.h, in fact things could be missing. If they were all *only* in _map.h, a simple grep of ''#define'' in *.c would be able to show you no #defines in any .c, and hence no bit definitions in any .c, meaning they all must be in _map.h I hate to look a gift horse in the mouth, and I realize it's rather obsessive-compulsive of me to complain when you're just giving people what they asked for, but I also look forward to a future release of fwlib that doesn't have duplicate #defines. Thanks again, Miles2011-05-17 3:45 AM
It is possible that they just need some time to better integrate the new file into the library. Probably they rushed it a bit because the pressure in this forum.
Anyway, thank you for the excellent news, I will integrate the new file in the next versions of my projects. Giovanni --- ChibiOS/RT2011-05-17 3:45 AM
That's great news. Thank you ST!
Steve.2011-05-17 3:45 AM
Thanks for that, your support is much appreciated.
Jan