2016-09-29 2:10 PM
Hi,
I got two STM32 board which I'm trying to send data through one and receive it on the other board through bluetooth. I have configured the HC-05 as master and it connects to the HC-6 successfully. The problem is the data i receive on the other board is not making any sense at all. When I use the same code and using a cable to send the data through the boards its working fine. I really appreciate if someone could help me with this problem, i have been stuck for over 2 days now and i have tried everything.. Here is my code for the TX board:void USART_Config(void);
void appInit(void){
init_GPIO(GPIOE, GPIO_Pin_All, GPIO_Mode_OUT, GPIO_Speed_25MHz, GPIO_OType_PP, GPIO_PuPd_UP);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE);
init_GPIO(GPIOC, GPIO_Pin_0, GPIO_Mode_AN, GPIO_Speed_25MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
init_GPIO(GPIOC, GPIO_Pin_1, GPIO_Mode_AN, GPIO_Speed_25MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
}
uint16_t read_ADC_new(ADC_TypeDef* ADCx){
ADC_SoftwareStartConv(ADCx);
while(ADC_GetFlagStatus(ADCx, ADC_FLAG_EOC) == RESET)
;
return ADC_GetConversionValue(ADCx);
}
void init_Any_ADC(ADC_TypeDef* ADCx,
uint32_t ADC_Resolution,
FunctionalState ADC_ScanConvMode,
FunctionalState ADC_ContinuousConvMode,
uint32_t ADC_ExternalTrigConvEdge,
uint32_t ADC_ExternalTrigConv,
uint32_t ADC_DataAlign,
uint32_t ADC_NbrOfConversion){
ADC_InitTypeDef ADC_InitStructure;
ADC_DeInit();
ADC_InitStructure.ADC_Resolution = ADC_Resolution;
ADC_InitStructure.ADC_ScanConvMode = ADC_ScanConvMode;
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign;
ADC_InitStructure.ADC_NbrOfConversion = ADC_NbrOfConversion;
ADC_Init(ADCx, &ADC_InitStructure);
}
void ADC_Config(void){
initCommon_ADC(ADC_Mode_Independent, ADC_Prescaler_Div2, ADC_DMAAccessMode_Disabled, ADC_TwoSamplingDelay_10Cycles);
init_Any_ADC(ADC2, ADC_Resolution_6b, DISABLE, ENABLE, ADC_ExternalTrigConvEdge_None, ADC_ExternalTrigConv_T1_CC1,
ADC_DataAlign_Right, 1);
init_Any_ADC(ADC3, ADC_Resolution_6b, DISABLE, ENABLE, ADC_ExternalTrigConvEdge_None, ADC_ExternalTrigConv_T2_CC3,
ADC_DataAlign_Right, 1);
ADC_Cmd(ADC2, ENABLE);
ADC_Cmd(ADC3, ENABLE);
ADC_RegularChannelConfig(ADC2, ADC_Channel_10, 1, ADC_SampleTime_144Cycles);
ADC_RegularChannelConfig(ADC3, ADC_Channel_11, 1, ADC_SampleTime_144Cycles);
}
void USART_Config(void){
// Enable UART clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
// Connect USART(3) to pin0 OUTPUT (TX)
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_UART4);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
// Configure TX pin to alternative function with push-pull
init_GPIO(GPIOA, GPIO_Pin_0, GPIO_Mode_AF, GPIO_Speed_2MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
init_GPIO(GPIOA, GPIO_Pin_2, GPIO_Mode_AF, GPIO_Speed_2MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
init_SCI(UART4, 9600, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx,
USART_HardwareFlowControl_None);
init_SCI(USART2, 9600, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx,
USART_HardwareFlowControl_None);
USART_Cmd(USART2, ENABLE);
}
void InitializeLEDs(){
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
init_GPIO(GPIOB, GPIO_Pin_4, GPIO_Mode_AF, GPIO_Speed_25MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
}
void sendString(char *s){
while(*s){
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, 0x01);
}
}
int main(int argc, char** argv){
appInit();
USART_Config();
ADC_Config();
while(1) {
uint16_t power = read_ADC_new(ADC2);
uint16_t steering = read_ADC_new(ADC3);
power = (power >> 6) / 8; // 3 bitar gas
steering = steering / 2; // 5 bitar styrning
//uint8_t data = 0xAA;
uint8_t data = ((power << 5) + steering);
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2, data);
}
}
And here is the code for RX board:
void appInit(void)
{
init_GPIO(GPIOE, GPIO_Pin_All, GPIO_Mode_OUT, GPIO_Speed_2MHz, GPIO_OType_PP, GPIO_PuPd_UP);
}
void USART_Config(void)
{ //Enable clock for GPIOC
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
// Enable UART clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
// Connect UaRT4 to pin11 INPUT (RX)
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_USART2);
// Configure RX pin to alternative function with push-pull
init_GPIO(GPIOD, GPIO_Pin_6, GPIO_Mode_AF, GPIO_Speed_2MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
//Configure UART4 with correct paramaters.
init_SCI(USART2, 9600, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Rx,
USART_HardwareFlowControl_None);
//Enable UART4
USART_Cmd(USART2, ENABLE);
}
//Function to init TIM
void Init_Timer(int period)
{
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
TIM_TimeBaseInitTypeDef TIM_Structure;
TIM_Structure.TIM_Prescaler = 100;
TIM_Structure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_Structure.TIM_Period = period;
TIM_Structure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_Structure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM3, &TIM_Structure);
TIM_Cmd(TIM3, ENABLE);
}
//Function to set TIM to pwm mode.
void Init_PWM(int pulse)
{
TIM_OCInitTypeDef OC_Init = {0,};
OC_Init.TIM_OCMode = TIM_OCMode_PWM1;
OC_Init.TIM_Pulse = pulse;
OC_Init.TIM_OutputState = TIM_OutputState_Enable;
OC_Init.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &OC_Init);
init_GPIO(GPIOB, GPIO_Pin_4, GPIO_Mode_AF, GPIO_Speed_100MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_TIM3);
}
void InitializeLEDs()
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
init_GPIO(GPIOB, GPIO_Pin_4, GPIO_Mode_AF, GPIO_Speed_2MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
// init_GPIO(GPIOB, GPIO_Pin_1, GPIO_Mode_AF, GPIO_Speed_25MHz, GPIO_OType_PP, GPIO_PuPd_NOPULL);
}
int main(int argc, char** argv)
{
// InitializeLEDs();
//11927
// max höger 880
// styrning idle 1200
// körning idle 1000;
Init_Timer(11700);
Init_PWM(1500);
appInit();
USART_Config();
unsigned char c;
uint16_t t = 1116;
while(1) {
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET);
uint8_t val = USART_ReceiveData(USART2);
write_GPIO_Byte(GPIOE, LOW_BYTE, val);
}
}
#stm32 #bluetooth #- #stm32f030-!usart
2016-09-29 6:29 PM
You'd want to confirm the configuration/settings in each of the modules. Check baud rates with a scope, send 0x55 (U) patterns in a stream.
I'd suggest breaking the problem in two, use a PC connected BlueTooth module, and use it to confirm reception of data from the transmitter, and then acting as the transmitter to the receiving module.2016-09-30 4:18 AM
Hi Clive,
I connected one of the module to my Android phone and used a BlueTooth terminal to recieve data. I was sending like you said (0x55) from my board and what i recieve was 1c.. It doesnt matter if i change what im sending, im still recieving 1c.. The baud rate is correct at 9600