HardFault exception problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-23 11:33 PM
I make boot loader for jump to 0x08020000
And, I make program that start from 0x08020000, also same vector table address(0x08020000)
It works well, but sometimes(when program modified), it doesn't work
I use debugger, and get result below
//Fault exception viewer
HardFault exception.
The processor has escalated a configurable-priority exception to HardFault.
A precise data access error has occurred (CFSR.PRECISERR, BFAR) at data address 0x1fff8001.
Exception occured at PC = 0x80216ae, LR = 0x802b61d
See the call stack for more information.
//Debug Log
The stack pointer for stack 'CSTACK' (currently 0x200025C8) is outside the stack range (0x20009170 to 0x2000A170)
What is the problem?
Can you help me?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 12:09 AM
Have you tried to pinpoint the exact location (instruction) where the fault happens ?
Perhaps you tried to access peripherals not yet enabled ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 1:23 AM
Thank you AvaTar
But, I don't know what i can
I try to debug program only, it works well.
I try to set program address and vector table 0x0800 0000, it works well.
Therefore, I guess set register or interrupt error when jump from 0x08000000(boot loader) to 0x08020000(program)
I made program it works well,
And, add 2lines in any function, uint8_t buf[10] and memset ( buf, 0x00, 10)
then, program halt and same issue
It work well at 0x08000000 or 0x08020000 starting by debugger
It's so hard to solve
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 1:33 AM
Does the application set it's own vector table properly ?
Sounds like it uses the BL table.
In a similar application I have, the application sets the VTOR as one of the very first things in the reset handler.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 2:07 AM
I set icf file
define symbol __ICFEDIT_intvec_start__ = 0x08020000;
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x08020000;
define symbol __ICFEDIT_region_ROM_end__ = 0x080FFFFF;
I set stm32f2xx.c file
​#define VECT_TAB_OFFSET 0x20000
void SystemInit(void)
{
RCC->CR |= (uint32_t)0x00000001;
RCC->CFGR = 0x00000000;
RCC->CR &= (uint32_t)0xFEF6FFFF;
RCC->PLLCFGR = 0x24003010;
RCC->CR &= (uint32_t)0xFFFBFFFF;
RCC->CIR = 0x00000000;
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
}
#define FLASH_BASE 0x08000000U /*!< FLASH(up to 1 MB) base address in the alias region */
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 2:24 AM
Our BL-loaded firmware does this as the very first thing in the reset handler:
; relocate the VTAB to the location in the firmware (0x30000)
LDR R0, =__vector_table ; get pointer to vector table
LDR R1, =0xE000ED08 ; store the table address to NVIC VTOR register
STR R0, [R1] ; Vector Table Relocation in Internal FLASH
IAR WB, but for another (non-ST) MCU, though. And your application project needs to map the vector table there, of course.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 2:40 AM
Where should I insert that code?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 2:57 AM
I showed this code just as example. I hope you understood that addresses do not match - it is actually for a Cypress FM4 MCU.
> Where should I insert that code?
For our application, we created a derived startup code (using the IAR-supplied "startup_***.s" as starting point), which relocates the vector table, and sets the stack pointer from that table.
Afterwards, SystemInit and __iar_program_start are called (as usual).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-10-24 3:20 AM
Ok, I see, I know that is example code (vtor 0x30000)
This is my startup code
-----------------------------------------------------------------
MODULE ?cstartup
;; Forward declaration of sections.
SECTION CSTACK:DATA:NOROOT(3)
SECTION .intvec:CODE:NOROOT(2)
EXTERN __iar_program_start
EXTERN SystemInit
PUBLIC __vector_table
DATA
__vector_table
DCD sfe(CSTACK)
DCD Reset_Handler ; Reset Handler
DCD NMI_Handler ; NMI Handler
....
-------------
SystemInit() calls here, and SystemInit() set vtor