2019-04-16 1:02 AM
I used to send AT command to a module with HAL_UART_Transmit():
void send_uart(char * buffer)
{
uint16_t buffer_size = strlen(buffer);
uint8_t CRLFbuff[] = "\r\n";
HAL_UART_Transmit(&hlpuart1, CRLFbuff, 2, 0xFF); // ok
HAL_UART_Transmit(&hlpuart1, (uint8_t *)buffer, buffer_size, 0xFF); // ok
HAL_UART_Transmit(&hlpuart1, CRLFbuff, 2, 0xFF); // ok
}and receive answer with HAL_UART_Receive_IT() byte per byte:
HAL_UART_Receive_IT(&hlpuart1, &Rx_data, 1);
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == LPUART1){ // Current UART
if (Rx_indx + 1 > rx_buffer_size){
Rx_indx = 0;
}
if (Rx_data != 0x0A){ // If received data different from LF
Rx_Buffer[Rx_indx++] = Rx_data; // Add data to Rx_Buffer
}
else {
Rx_indx = 0;
Transfer_cplt++;//transfer complete, data is ready to read
}
HAL_UART_Receive_IT(&hlpuart1, &Rx_data, 1); //activate UART receive interrupt every time
}
}And this is working well at 9600 in nominal TX/RX. But if I send bad data to the module it sends immediately "ERROR: parse error" while my STM32L031 is still transmitting. This as the effect of killing my RX interrupt. Instead of being HAL_UART_STATE_BUSY_RX the UART->RxState switches to HAL_UART_STATE_READY and RX interrupt is never triggered (transmit part still works good).
I changed my transmit code to HAL_UART_Transmit_IT (with little rework) and this behavior is not observed (works well).
Is this normal ?
Solved! Go to Solution.
2022-10-31 9:03 AM
I know, I'm late!
Thanks a lot for your explanations. I'm using the STM32Cube_FW_G4_V1.5.1. In the functions HAL_UART_Transmit_IT and the HAL_UART_Receive_IT containt the macro __HAL_LOCK().
If I wand to process TX and RX with variable length. I would implement the RxCallback like this.
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
// Store the recieve character to the next layer
// Restart Receive
HAL_StatusTypeDef status = HAL_UART_Receive_IT(&huart1, UART1_rxBuffer, 1);
if (status != HAL_OK) {
__NOP(); // Only for setting breakpoint
}
}And somewhere in the main loop (for example) I would like to trigger a TX-Message like this.
...
HAL_StatusTypeDef status = HAL_UART_Transmit_IT(&huart1, UART1_txBuffer, length);
if(status!=HAL_OK) {
__NOP(); // Only for setting breakpoint
}
...Due the asynchronous processing there is a race condition by the __HAL_LOCK().
What did I miss? Thank you for your help.