cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_UART_Transmit_DMA

papageno
Associate III

Hello dear experts,

I am trying to send a binary 32bits over the uart3 using either HAL_UART3_Transmit (polling, It or DMA).

1- sending roughly the 32bits with a length of 4 in the function parameters does not work.

2 -sorting the 32bits data in a 8bits array with >> and & and passing the array @ with a lenth of 4 does not work.

3- using a loop and sending the 4 bytes one by one with a length of 1 works whatever the mode but maybe the most efficient considering the time.

4- the following code sends correctly 3 bytes out of 4... the last one is corrupted. Dont understand why, on the scope, 81 appears as 08

uint32_t data = 0x815533AA;

uint8_t dataArray[4];

dataArray[0] = data & 0x000000FF;

dataArray[1] = (data & 0x0000FF00) >> 8;

dataArray[2] = (data & 0x00FF0000) >> 16;

dataArray[3] = (data & 0xFF000000) >> 24;

HAL_UART_Transmit_DMA(&huart3, (uint8_t*)dataArray, 4);

NB: the last byte is always 0x08 whatever the value; i am using DAM1 stream3 mode normal data with byte for peripheral and memory.

I think i am missing an important point in DMA transfers....

Thanks for your help.

Pap

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
TDK
Super User

Include your part number.

Don't send local variables out through DMA. Since DMA operates asynchronously, the variables go out of scope before it completes. Use a global array, or otherwise ensure the array remains valid until DMA is complete.

If you feel a post has answered your question, please click "Accept as Solution".
papageno
Associate III

Thanks TDK, Got it! excellent suggestion ! I thought that DMA transfer were faster. Do you think I also need to check the function returned value and also the serial state ?

regards.

TDK
Super User

> I thought that DMA transfer were faster.

The UART speed is constant. Using DMA just means it goes on in the background while your CPU is off doing other things.

> Do you think I also need to check the function returned value and also the serial state ?

I would. Easy enough to do and it can help you find bugs faster than if you let the function fail silently.

If you feel a post has answered your question, please click "Accept as Solution".
papageno
Associate III

Using the global variables as proposed, it worked correctly at speed around 961Kbits/s on uart3 but when I try to increase the baud rate up to 1.843Mbits/s the last byte is corrupted. I also noticed that the returned value of HAL_UART_Transmit_DMA() is correct but testing the uart status stays stuck in the while loop....

while (HAL_UART_GetState(&huart3) != HAL_UART_STATE_READY)

{

}

Any suggestion for both problems (speed and status)?

I thank you in advance.

Pap

Using the global variables as proposed, it worked correctly at speed around 961Kbits/s on uart3 but when I try to increase the baud rate up to 1.843Mbits/s the last byte is corrupted. I also noticed that the returned value of HAL_UART_Transmit_DMA() is correct but testing the uart status stays stuck in the while loop....

while (HAL_UART_GetState(&huart3) != HAL_UART_STATE_READY)

{

}

Any suggestion for both problems (speed and status)?

I thank you in advance.

Pap

TDK
Super User

I would find a HAL example using DMA UART and go from there.

The State should get changed back in the DMA complete interrupt.

If you feel a post has answered your question, please click "Accept as Solution".

dear TDk,

i can se ethat the uart3 state is HAL_UART_STATE_BUSY_TX and appaarently it never switches to HAL_UART_STATE_READY so I stay stuck in the isr callback and no data is sent. Not testing that value produces a corrupted last byte on the uart3. Is there any speed problem with uart3 to your knowledge.

regards,

pap