2020-01-08 11:58 AM
Hi there!
I hope someone can help me. Afther a couple of years i start again to program the STM32 microcontroller (STM32F051). I need the use a UART for trasmit and receive data. For the trasmission no problem work weel ( i use the interrup HAL functions). My problem is when i want receive a data where i do to write the HAL_UART_Receive_IT function ? before a while or inside the while ? and why ? i'm confused. Someone know a good book or tutorial can hel me to understand the hal library ?
thank you soo much
Sergio
2020-01-08 12:15 PM
Well until someone has something better, try Tilen's https://github.com/MaJerle
2020-01-08 1:01 PM
HAL_UART_Receive_IT prepares the hardware for receiving a buffer of fixed length. After the buffer is filled, the interrupt handler calls HAL_UART_RxCpltCallback, you implement that callback. At the end of the HAL_UART_RxCpltCallback callback, you will probably call HAL_UART_Receive_IT again to prepare for the next buffer.
This simple implementation takes only one char per interrupt:
char ch;
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Receive_IT( &huart2, &ch, 1 );
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
...and
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
// do something with ch
HAL_UART_Receive_IT( &huart2, &ch, 1 );
}Note, that the USART2 global interrupt must be enabled in your project.
Todo: add error checking and handling.
hth
KnarfB
2020-01-08 10:59 PM
Thank you soo much. If i understand this stuff work for I2c bus and Spi
Sergio
2020-01-09 9:50 AM
:grinning_face: :grinning_face: wonderful finally work just one question inside a HAL_UART_RxCpltCallback is necessary write HAL_UART_Receive_IT( &huart2, &ch, 1 ); or i can just reset some flags ? and the answert is yes just reset some flags how ?
Thank you
Sergio
2020-01-09 11:40 AM
Don't know, sorry. You may set a breakpoint in HAL_UART_RxCpltCallback, step into HAL_UART_Receive_IT and find out.
hth
KnarfB