Skip to main content
skon.1
Associate III
July 24, 2020
Question

HAL_UART_Receive doesn't block execution

  • July 24, 2020
  • 9 replies
  • 2998 views

Helllo,

I'm working on the NUCLEO-F722ZE EVB.

I want my code to wait for a character to be received from UART 3 and do nothing.

This is what I wrote:

unibt8_t received_character = 0 ;
HAL_UART_Receive(&huart3, received_character, 1,1000) ;

From what I understand "HAL_UART_Receive" is a blocking function so it should block the code execution until a character is received. But for some reason my code doesn't stop and proceeds to the next line although no data was sent to the UART.

What am I doing wrong ?

This topic has been closed for replies.

9 replies

TDK
July 24, 2020

> until a character is received.

Or until the timeout occurs. You have specified a 1000ms timeout.

The return value will be HAL_TIMEOUT in this case, which you can catch and handle appropriately.

"If you feel a post has answered your question, please click ""Accept as Solution""."
skon.1
skon.1Author
Associate III
July 24, 2020

How can I make it wait indefinitely ?

TDK
July 24, 2020

0xFFFFFFFE gives you a timeout of 50 days.

Otherwise you need a loop:

while (HAL_UART_Receive(&huart3, &received_character, 1, 1000) == HAL_TIMEOUT);

Your code also has typos.

unibt8_t received_character = 0 ; // <-- unibt8_t is not a type
HAL_UART_Receive(&huart3, received_character, 1,1000) ; // <-- this writes to memory address 0. missing a & character

"If you feel a post has answered your question, please click ""Accept as Solution""."
skon.1
skon.1Author
Associate III
July 24, 2020

Thanks.

What did you mean by:

"<-- unibt8_t is not a type" ?

S.Ma
Principal
July 25, 2020

Unless you really do expect only a single byte, I would strongly recommend at least to use interrupts which anyway are part of normal practice in microcontroller world. If you don't want interrupts and don't care the latency, use DMA with cyclic buffer (say 1024 bytes) so you can see what you receive in the buffer. Size the buffer so that its size don't overflow with the worst case polling delay.

skon.1
skon.1Author
Associate III
July 25, 2020

Yes, I get your point.

But for this peripheral - the single byte is a requirement.

I want the user to press on a single keyboard character to navigate in an internal menu.

I have another UART in the design that's intended to send/receive chunks of data with another device.

For that UART it'll probably be wise to use a DMA.

Are there official ST examples that showcase the usage of HAL functions ?

S.Ma
Principal
July 25, 2020

Go for interrupts and fill up the callback isr portion. That's futureproof. In polling monitor for the rxne flag prior to read the data byte.

skon.1
skon.1Author
Associate III
July 25, 2020

Can you please post an example for this ?

TDK
July 25, 2020

> Are there official ST examples that showcase the usage of HAL functions ?

Here are three of many:

https://github.com/STMicroelectronics/STM32CubeF7/tree/master/Projects/STM32746G-Discovery/Examples/UART

"If you feel a post has answered your question, please click ""Accept as Solution""."