Skip to main content
David Littell
Senior II
May 30, 2018 7:31 PM UTC
Question

HAL_GPIO_TogglePin() not thread-safe

Posted on May 30, 2018 at 21:31

STM32Cube_FW_F7_V1.11.0's HAL_GPIO_TogglePin() appears broken in a multi-threaded environment:

void HAL_GPIO_TogglePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin)

{

  /* Check the parameters */

  assert_param(IS_GPIO_PIN(GPIO_Pin));

   GPIOx->ODR ^= GPIO_Pin;

}

One fix might be:

void HAL_GPIO_TogglePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin)

{

  /* Check the parameters */

  assert_param(IS_GPIO_PIN(GPIO_Pin));

  if( (GPIOx->ODR & GPIO_Pin) != 0x0 )

    {

      GPIOx->BSRR = ((uint32_t) GPIO_Pin) << 16;   /* Set a BSRR.BRx bit so the GPIO goes low. */

    }

  else   /* the GPIO should be set high... */

    {

      GPIOx->BSRR = (uint32_t) GPIO_Pin;   /* Set a BSRR.BSx bit so the GPIO goes high. */

    }

}

I suspect all the HAL's may suffer from this...

    This topic has been closed for replies.

    5 replies

    Tilen MAJERLE
    ST Employee
    May 30, 2018 7:35 PM UTC
    Posted on May 30, 2018 at 21:35

    Hello,

    method you provided is not thread safe aswell. The only thread safe option is to use mutex/sem before calling TogglePin function. Hardware does not support toggling with single instruction like set/reset operation with BSRR register.

    Best regards,

    Tilen

    waclawek.jan
    Super User
    May 30, 2018 9:44 PM UTC
    Posted on May 30, 2018 at 21:44

    Maybe David's solution is not thread safe in an absolute meaning of the word, as two threads manipulating the same bit may get into conflict. But, isn't that a bit pathologic scenario?

    OTOH, the original solution is plain wrong, as it will influence other bits in the same GPIO port.

    JW

    Tilen MAJERLE
    ST Employee
    May 30, 2018 9:55 PM UTC
    Posted on May 30, 2018 at 21:55

    Hello

    Waclawek.Jan

    ‌,

    I do agree with you that itis better, but it is technically and theoretically still wrong. It may happen you have wrong output levels.

    Best regards,

    Tilen

    Garnett.Robert
    Senior III
    Sep 21, 2023 12:50 PM UTC

    Hi,

    If you have code that must complete uninterrupted shouldn't you put it in a critical section, i.e. interrupts disabled?

    Toggling a pin from two different threads seems an odd thing to do. I can imagine having one thread turning the pin on and another turning it off and vice versa, but toggling?

    Regards

    Rob