Posted on December 16, 2015 at 04:39/**
* @brief Clear the DMA Stream pending flags.
* @param __HANDLE__: DMA handle
* @param __FLAG__: specifies the flag to clear.
* This parameter can be any combination of the following values:
* @arg DMA_FLAG_TCIFx: Transfer complete flag.
* @arg DMA_FLAG_HTIFx: Half transfer complete flag.
* @arg DMA_FLAG_TEIFx: Transfer error flag.
* @arg DMA_FLAG_DMEIFx: Direct mode error flag.
* @arg DMA_FLAG_FEIFx: FIFO error flag.
* Where x can be 0_4, 1_5, 2_6 or 3_7 to select the DMA Stream flag.
* @retval None
*/
#define __HAL_DMA_CLEAR_FLAG(__HANDLE__, __FLAG__) \
(((uint32_t)((__HANDLE__)->Instance) > (uint32_t)DMA2_Stream3)? (DMA2->HIFCR = (__FLAG__)) :\
((uint32_t)((__HANDLE__)->Instance) > (uint32_t)DMA1_Stream7)? (DMA2->LIFCR = (__FLAG__)) :\
((uint32_t)((__HANDLE__)->Instance) > (uint32_t)DMA1_Stream3)? (DMA1->HIFCR = (__FLAG__)) : (DMA1->LIFCR = (__FLAG__)))
I don't understand how the code from ST HAL can clear the flag?