HAL_Delay stuck SysTick not triggered, workaround for stm32f105
- August 28, 2023
- 7 replies
- 6845 views
Hi,
I have scoured the web for a solution to this problem, but I cannot find one, typically the replies are the same, but the solution is never found. I have tried every other solution you will find.
I was playing around with the cube mx trying to solve my problem with this, and I'm not sure what changed, but the cube mx generated a program which actually made HAL_Delay work correctly.
I have used the STM32CubeIDE with CubeMX generated code for many projects in the past with relatively no issues.
- STM32F105
- STLINK_V3
- Firmware Package: STM32Cube FW_F1 V1.8.5
- STM32CubeIDE version 1.13.0
- MXCube Version 6.9
The Problem:
To summarise the problem, the application will freeze at HAL_Delay();
The reason for this is because within the file stm32f1xx_t.c , the SysTick_Handler will not be called, and hence HAL_IncTick(); will also never increment the uwTick counter. Clearly the Systick Interrupt isn't being triggered.
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}
The following call stack will be shown when you try and Step-Over HAL_Delay(); while debugging.
Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
uwTickPrio() at 0x20000004
<signal handler called>() at 0xfffffff9
HAL_GetTick() at stm32f1xx_hal.c:307 0x8000806
HAL_Delay() at stm32f1xx_hal.c:382 0x800083c
main() at main.c:98 0x8000546
Work Around:
I have found that for whatever reason the file system_stm32f1xx.c (located in Core/Src is related. In my working.rar which I have attached you will find that the system_stm32f1xx.c file is different to the not working.rar
If I copy the system_stm32f1xx.c file from the working project into the not working project, it will compile and debug correctly. There is major differences between the files but I do not understand them.
Perhaps someone with more experience with the inners of how the ST generation behaves can shed some light on why this would happen.