cancel
Showing results for 
Search instead for 
Did you mean: 

H755 / ADC3 / DMA

UBöke.1
Associate II

Hello,

I'm desperate. Just want to concvert some data with the ADC3 with DMA on a H755.

No chance! DMA doesn't work, and even a cyclic sample only produces the right values for the first turn. After that, only max. resolution is returned. 12 bit => 0x800 as the result.

Can anybody help ?

7 REPLIES 7
AScha.3
Chief II

most times same problem: no cache management.

try: switch off D-cache (= not enable d-cache )

If you feel a post has answered your question, please click "Accept as Solution".

I checked it => CCache and DCache OFF !

ICache... not CCache

 

UBöke.1
Associate II

More or less solved.

and..it was ..?

If you feel a post has answered your question, please click "Accept as Solution".
UBöke.1
Associate II

Ich weiß es wirklich nicht. Ich habe alles gelöscht, STM-Cube deinstalliert, neu installiert und alle HAL_ Treiber neu aus dem Netz geladen, noch einmal alles eingestellt. Und irgendwie funktioniert es jetzt so, wie es soll.

ok, also eclipse/CubeIDE/STM  standard Verfahren .

aach, is on Win ?    then Windows standard. 

If you feel a post has answered your question, please click "Accept as Solution".