li.media.document-lightbox.error.message
2018-01-25 9:47 PM
I am interfacing sim 908 module with stm32f407VG discovery board. I programmed using CubeMx . Using AT commands I am able to transmit message to my phone via gsm module. The problem is I am not able to receive the message from my phone to the gsm module. Code is attached here. Please help.
2018-01-26 5:24 AM
Bit of a fail there at providing the code that actually talks to the modem, or that checks/reads the SMS
Don't attach multiple files individually. ZIP up what you want to share, and attach ONE file with ALL the pieces.