cancel
Showing results for 
Search instead for 
Did you mean: 

Try to get spi communication up and running between a stm32l-discovery board and a nRF24L01

Helen Wang
Associate
Posted on January 26, 2018 at 11:04

I am currently trying to get spi communication up and running between a stm32l-discovery board (uses STM32L152RCT6 mcu) and a nRF24L01(

http://www.kynix.com/Detail/114168/NRF24Lhtml

) module. I have the module connected to the discovery board via the following pins (apart from the 3v and gnd):

// CS = PB12 (SPI_NSS)// SCK = PB13 (SPI_SCK)// MI = PB14 (SPI_MISO)// MO = PB15 (SPI_MOSI)// CE = PD2

My uart gives the following output:

nrf radio example

set 1500us timeout: (LOW)

It is currently stuck there because the spi registers don't seem to update and I'm not sure if I configured something wrong. My biggest problem though is that I'm not sure how I can debug this further? I'm still very new to stm

Here is my current code:

#include 'stm32l1xx_conf.h'#include <stdio.h>#include <stdlib.h>#include <string.h>#include <stdarg.h>/* Memory Map */#define CONFIG 0x00#define EN_AA 0x01#define EN_RXADDR 0x02#define SETUP_AW 0x03#define SETUP_RETR 0x04#define RF_CH 0x05#define RF_SETUP 0x06#define STATUS 0x07#define OBSERVE_TX 0x08#define CD 0x09#define RX_ADDR_P0 0x0A#define RX_ADDR_P1 0x0B#define RX_ADDR_P2 0x0C#define RX_ADDR_P3 0x0D#define RX_ADDR_P4 0x0E#define RX_ADDR_P5 0x0F#define TX_ADDR 0x10#define RX_PW_P0 0x11#define RX_PW_P1 0x12#define RX_PW_P2 0x13#define RX_PW_P3 0x14#define RX_PW_P4 0x15#define RX_PW_P5 0x16#define FIFO_STATUS 0x17#define DYNPD 0x1C#define FEATURE 0x1D/* Bit Mnemonics */#define MASK_RX_DR 6#define MASK_TX_DS 5#define MASK_MAX_RT 4#define EN_CRC 3#define CRCO 2#define PWR_UP 1#define PRIM_RX 0#define ENAA_P5 5#define ENAA_P4 4#define ENAA_P3 3#define ENAA_P2 2#define ENAA_P1 1#define ENAA_P0 0#define ERX_P5 5#define ERX_P4 4#define ERX_P3 3#define ERX_P2 2#define ERX_P1 1#define ERX_P0 0#define AW 0#define ARD 4#define ARC 0#define PLL_LOCK 4#define RF_DR 3#define RF_PWR 6#define RX_DR 6#define TX_DS 5#define MAX_RT 4#define RX_P_NO 1#define TX_FULL 0#define PLOS_CNT 4#define ARC_CNT 0#define TX_REUSE 6#define FIFO_FULL 5#define TX_EMPTY 4#define RX_FULL 1#define RX_EMPTY 0#define DPL_P5 5#define DPL_P4 4#define DPL_P3 3#define DPL_P2 2#define DPL_P1 1#define DPL_P0 0#define EN_DPL 2#define EN_ACK_PAY 1#define EN_DYN_ACK 0/* Instruction Mnemonics */#define R_REGISTER 0x00#define W_REGISTER 0x20#define REGISTER_MASK 0x1F#define ACTIVATE 0x50#define R_RX_PL_WID 0x60#define R_RX_PAYLOAD 0x61#define W_TX_PAYLOAD 0xA0#define W_ACK_PAYLOAD 0xA8#define FLUSH_TX 0xE1#define FLUSH_RX 0xE2#define REUSE_TX_PL 0xE3#define NOP 0xFF/* Non-P omissions */#define LNA_HCURR 0/* P model memory Map */#define RPD 0x09/* P model bit Mnemonics */#define RF_DR_LOW 5#define RF_DR_HIGH 3#define RF_PWR_LOW 1#define RF_PWR_HIGH 2#define SPI_CS_HIGH GPIO_WriteBit(GPIOB, GPIO_Pin_12, Bit_SET);#define SPI_CS_LOW GPIO_WriteBit(GPIOB, GPIO_Pin_12, Bit_RESET);#define NRF_CE_HIGH GPIO_WriteBit(GPIOD, GPIO_Pin_2, Bit_SET);#define NRF_CE_LOW GPIO_WriteBit(GPIOD, GPIO_Pin_2, Bit_RESET);void usart_write(uint8_t ch){ USART_SendData(USART1, (uint8_t) ch); while(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET) { }} void usart_print( char *msg ){ int len = strlen( msg ); for ( int c = 0; c < len; c++ ) usart_write( (uint8_t)*msg++ );}void delay( int a ){ volatile int i, j; for ( i = 0; i < a; i++ ) { j++; }} uint16_t spi_transfer( uint16_t data ){ while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); usart_print( '(senddata)' ); SPI_I2S_SendData( SPI2, data ); usart_print( '(wait)' ); // wait for transfer to finish while (SPI_I2S_GetFlagStatus( SPI2, SPI_I2S_FLAG_RXNE ) == RESET); usart_print( '(recvdata)' ); return SPI_I2S_ReceiveData(SPI2);}void spi_send( uint16_t data ){ // wait for transfer to finish while ( SPI_I2S_GetFlagStatus( SPI2, SPI_I2S_FLAG_TXE ) == RESET ); SPI_I2S_SendData( SPI2, data );}uint16_t spi_read(void){ // wait for transfer to finish while ( SPI_I2S_GetFlagStatus( SPI2, SPI_I2S_FLAG_RXNE ) == RESET ); return SPI_I2S_ReceiveData(SPI2);}uint16_t write_register_data(uint8_t reg, const uint8_t* buff, uint8_t len ){ uint16_t status; SPI_CS_LOW; status = spi_transfer( W_REGISTER | ( REGISTER_MASK & reg ) ); while ( len-- ) { spi_transfer(*buff++); } SPI_CS_HIGH; return status;}uint16_t read_register_data(uint8_t reg, uint8_t* buff, uint8_t len ){ uint16_t status; SPI_CS_LOW; status = spi_transfer( W_REGISTER | ( REGISTER_MASK & reg ) ); while ( len-- ) { *buff++ = spi_transfer(0xff); } SPI_CS_HIGH; return status;}uint16_t write_register_value(uint8_t reg, uint8_t value){ uint16_t status; usart_print( '(LOW)'); SPI_CS_LOW; status = spi_transfer(W_REGISTER | ( REGISTER_MASK & reg ) ); spi_transfer( value ); usart_print( '(HIGH)'); SPI_CS_HIGH; return status;}uint16_t read_register_value(uint8_t reg){ uint16_t status; SPI_CS_LOW; status = spi_transfer( W_REGISTER | ( REGISTER_MASK & reg ) ); spi_transfer( 0xff ); SPI_CS_HIGH; return status;} int main(void) { GPIO_InitTypeDef gpio_init; USART_InitTypeDef usart_init; USART_ClockInitTypeDef usart_clk_init; SPI_InitTypeDef spi_init; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOD, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); // spi // CS = PB12 (SPI_NSS) // SCK = PB13 (SPI_SCK) // MI = PB14 (SPI_MISO) // MO = PB15 (SPI_MOSI) // CE = PD2 gpio_init.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; gpio_init.GPIO_Mode = GPIO_Mode_AF; gpio_init.GPIO_Speed = GPIO_Speed_40MHz; gpio_init.GPIO_OType = GPIO_OType_PP; gpio_init.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &gpio_init); gpio_init.GPIO_Pin = GPIO_Pin_12; gpio_init.GPIO_Mode = GPIO_Mode_OUT; gpio_init.GPIO_Speed = GPIO_Speed_40MHz; gpio_init.GPIO_OType = GPIO_OType_PP; gpio_init.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &gpio_init); GPIO_PinAFConfig( GPIOB, GPIO_PinSource13, GPIO_AF_SPI2 ); GPIO_PinAFConfig( GPIOB, GPIO_PinSource14, GPIO_AF_SPI2 ); GPIO_PinAFConfig( GPIOB, GPIO_PinSource15, GPIO_AF_SPI2 ); gpio_init.GPIO_Pin = GPIO_Pin_2; gpio_init.GPIO_Mode = GPIO_Mode_OUT; gpio_init.GPIO_Speed = GPIO_Speed_40MHz; gpio_init.GPIO_OType = GPIO_OType_PP; gpio_init.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD, &gpio_init); SPI_StructInit(&spi_init); spi_init.SPI_Direction = SPI_Direction_2Lines_FullDuplex; spi_init.SPI_Mode = SPI_Mode_Master; spi_init.SPI_DataSize = SPI_DataSize_8b; spi_init.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; spi_init.SPI_NSS = SPI_NSS_Soft; spi_init.SPI_CPOL = SPI_CPOL_Low; spi_init.SPI_CPHA = SPI_CPHA_1Edge; spi_init.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI2, &spi_init); SPI_Cmd(SPI2, ENABLE); SPI_CS_HIGH; NRF_CE_LOW; // uart // PA9 = Tx, PA10 = Rx gpio_init.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; gpio_init.GPIO_Mode = GPIO_Mode_AF; gpio_init.GPIO_Speed = GPIO_Speed_40MHz; gpio_init.GPIO_OType = GPIO_OType_PP; gpio_init.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &gpio_init); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); USART_ClockStructInit(&usart_clk_init); USART_ClockInit(USART1, &usart_clk_init); usart_init.USART_BaudRate = 9600; usart_init.USART_WordLength = USART_WordLength_8b; usart_init.USART_StopBits = USART_StopBits_1; usart_init.USART_Parity = USART_Parity_No ; usart_init.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; usart_init.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART1, &usart_init); USART_Cmd(USART1,ENABLE); while(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET) {} usart_print( 'nrf radio test\r\n' ); delay(50000); usart_print( 'set 1500us timeout: ' ); uint16_t status = write_register_value(SETUP_RETR,(4 << ARD) | (15 << ARC)); usart_write( status ); usart_print( '\r\n' ); usart_print( 'begin\r\n' ); while (1) { } return 0;}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0