cancel
Showing results for 
Search instead for 
Did you mean: 

gsm 908 interfacing with stm32f407VG discovery board.

palak shrivastava
Associate
Posted on January 26, 2018 at 06:47

I am interfacing sim 908 module with stm32f407VG discovery board. I programmed using CubeMx . Using AT commands I am able to transmit message to my phone via gsm module. The problem is I am not able to receive the message from my phone to the gsm module. Code is attached here. Please help.

1 REPLY 1
Clive1 (HNL)
Senior II
Posted on January 26, 2018 at 14:24

Bit of a fail there at providing the code that actually talks to the modem, or that checks/reads the SMS

Don't attach multiple files individually. ZIP up what you want to share, and attach ONE file with ALL the pieces.