cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO to ADC channel mapping in STM32F105RBT.

DSimo.1
Associate

Hello,

I'm currently working on an application using STM32F105 uC.

I want to use some GPIO as analog input, so I need to use the ADC converter.

It seems that each channel is linked to one ADC channel. I have found some table with this mapping for other devices, but unfortunately I cannot find this table for this specific device.

(I attach STM32F3 a equivalence table just for your reference.)

With best regards,

Didac

0693W00000FA0r0QAD.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

They're in the pinout information in the datasheet. "ADC12_IN12" is shorthand for "ADC1_IN12 and ADC2_IN12".

0693W00000FA4PyQAL.png

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

They're in the pinout information in the datasheet. "ADC12_IN12" is shorthand for "ADC1_IN12 and ADC2_IN12".

0693W00000FA4PyQAL.png

If you feel a post has answered your question, please click "Accept as Solution".
DSimo.1
Associate

Hello,

Thank you very much.

I didn't notice.

WBR

Didac