cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO strange behaviour STM32F427

Bogdan
Senior
Posted on June 04, 2018 at 19:39

Hello,

i have a simple code where i just init some GPIO ports on a STM32F427VI  ( 100pin package).

The application controls via pin PA8 some transistor which switches on/off a relay after some delay...

I have noticed  if i configure PE2,  then PA8 does not work ( does not switch to HI).

If i comment out the red code shown bellow,  then PA8 works fine. Why is this? I have never encounter such problems with stm devices.

int main()

{

SystemInit();

GPIO_InitTypeDef GPIO_InitStruct;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOC| RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOB |RCC_AHB1Periph_GPIOE, ENABLE);// GPIOA & GPIOB clock enable

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_8;

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIOA->BSRRL = GPIO_Pin_3 ; // PA3 Hi 

GPIOA->BSRRH = GPIO_Pin_8; // PA8 Low 

for(uint32_t o=0; o<0xFFFFFF; o++) { } // some delay

for(uint32_t o=0; o<0xFFFFFF; o++) { } // some delay

GPIOA->BSRRL = GPIO_Pin_8; // PA8 hi

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_2;

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_Init(GPIOE, &GPIO_InitStruct);

return 0;

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Bogdan
Senior
Posted on June 04, 2018 at 22:34

So i found out the problem, after some debuging, it seems the mcu was reset by the POR supervisor.

  In my circuit i have a mic803-31D3VM3 on the ST reset pin which has a treshold voltage of 3.08V, so when i switched on the PA8 port,  due to poor filtering on the breadboard circuit, my supply voltage falls for some 10th's of us from 3.21 to 3.06volts

Posted on June 05, 2018 at 00:14

I use the MIC803, but at 2.9V and 1.2Seconds !