cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Read interact with GND or VCC

ULOK
Associate II

Hi,

I use STM32F103C8T6 a GPIO input pin to read a high or low signal from another GPIO output pin, and connect a 3Mohm resistor between two pins, and I notice touching GND with hand will influence the signal status, than I measure the resistance between GND and GPIO pin, it is around 10Mohm. I want to isolate the signal from GND interference, how should I do? I have to keep 3 Mohm resistor. will it be better if connect a capacitor between input pin and GND? or connect a large resistor in between?

1 ACCEPTED SOLUTION

Accepted Solutions
PGump.1
Senior III

Hi,

I would NOT recommend using GPIOs, directly, for that purpose.

In electronics, there are many Interface devices, for many purposes. I recommend finding one suitable for your application.

Many MCUs have integrated interfaces, perhaps there is a MCU with a suitable interface for your application...

I hope this helps.

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.

View solution in original post

5 REPLIES 5
Andrew Neil
Super User

@ULOK wrote:

I have to keep 3 Mohm resistor. 


Why??

At that level of resistance, it is to be expected that touching with a hand will be significant!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi, it is intended for hand detection, but touching GND will also be detected which is surprise. 3Mohm vs. 10(or 6Mohm), I want to increase the resistance to GND so that GND will not influence signal that much.

PGump.1
Senior III

Hi,

I would NOT recommend using GPIOs, directly, for that purpose.

In electronics, there are many Interface devices, for many purposes. I recommend finding one suitable for your application.

Many MCUs have integrated interfaces, perhaps there is a MCU with a suitable interface for your application...

I hope this helps.

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.

Hi Pedro,

Can you recommend a MCU with such interface? and better have CAN interface too. STM32 series will be good to use. Thank you!

look at capacitive touch sensing - many microcontrollers have it built in, and there are also external chips available.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.