Getting ST-LINK-V3 MODS to run after previous used of nucleoboards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 6:10 AM - edited ‎2024-03-13 6:10 AM
Hi,
i was hoping, that the Link-V3 would just work, after i used nucleo boards already. But i was dissapointed. I use the GDB server, and it says:
ST-Link enumeration failed
Error in initializing ST-LINK device.
Reason: ST-LINK DLL error.
I just checked a Nucleo board, and there is no problem.
The installation of the driver worked without errors.
Solved! Go to Solution.
- Labels:
-
STM32G4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 12:51 AM
IT WORKS!
While trying many things, i disconnectes NRST. But i still can program the target.
I had to enter the frequency in the gdb server comman line!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 6:34 AM
Can you connect with STM32CubeProgrammer? If not, at which stage does it fail? Does the ST-link show its serial number? Does the target voltage show up and is it valid?
Since this is custom hardware, was it ever working correctly or is this a first try? Does it have power, are pins connected correctly, is VCAP correct, etc?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 7:37 AM
It now works. I think i may have to turn / plugin the cables in a certain order.
But i now have this Error:
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 9:09 AM
I asked 6 questions, you answered 0 of them. If you want help by me, you're going to have to pitch in a bit more.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 10:37 AM - edited ‎2024-03-13 10:38 AM
Since the original error message is gone, i did not consider answering the question. But i do so now:
- I dont know i which way i should connect with the programmer.
- The GDB server now works, but running the cube programmer, it reads the ST-LINKV3 serial number and firmewareversion. It shows a voltage of 0.01V, but i confirmed, that the target has its 3.3V.
The current error massage is: "Error: No STM32 target found! If your product embeds Debug Authentication ..."
It is the first connect of this prototype. I was already wondering, why NRST was not on this ST-LINK.
I found out, that it is recognized, when the target is powered off.
What is VCAP?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 11:41 AM
Okay, it sounds like the computer can see the ST-Link okay and that the problem is between the st-link and the target mcu. Is that wired up correctly?
Since STM32CubeProgrammer reports that the target voltage is 0.01 V, perhaps the target isn't powered. I know you said that it is, but then we need to answer why STM32CubeProgrammer disagrees. Can you provide the schematic? Can you probe the T_VCC pin directly to see if it's reported?
T_NRST is pin 31 on that device and should be connected to NRST on the target chip.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 4:09 PM - edited ‎2024-03-13 4:10 PM
I have verified, that the labels are connected to the right pin. They also have a 5k resistor before the target.
I could verify, that there is a clock on the clock line, and some data on the DIO line.
One very interesting thing: there is a reset pulse right in the middle of a datapacket! That not so optimal.
When making the programmeradapterboard, i got a bit confused, because there is no NRST pin there. Also i could not find informations about how to connect it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 5:16 PM
The physically connectivity to the MCU and the involvement of the resistors would be a lot more helpful here.
The ST-LINK should be able to sample and report the target voltage correctly.
The connectivity to the MCU should be pretty direct and straight forward
NRST / NRESET
SWDIO
SWCLK
VCC to T_VCC to drive the target pins at the correct voltage
GND
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
‎2024-03-13 10:43 PM
What does the "T_" stand for?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-13 11:33 PM
I have now made more measurements:
The signal have the right levels without a T_VCC connection.