Function use in stm32 Library
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-10 4:33 AM
as you can see below , i am writing a function from stm32 library
void I2C_SendData(I2C_TypeDef* I2Cx, uint8_t Data)
the question is, can i use it in main file like
I2C_SendData(I2C1,(uint8_t*)data_t);
can i go from "uint8_t Data"" to ""(uint8_t*)data_t"
may i use pointer ?
Thanks
- Labels:
-
I2C
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-10 5:48 AM
You can't give it a pointer if it's expecting a value instead. You'll need to send values one at a time.
If you switch to the HAL library, you can send multiple bytes at once with HAL_I2C_Master_Transmit.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-10 10:29 AM
Thanks for your reply!
actually i have to transmit data to LCD 16X2, i know it works for HAL_I2C_Master_Transmit.
what do you mean sending values one at a time ? i write code below, can you kindly check
void lcd_send_cmd (char cmd)
{
char data_u, data_l;
uint8_t data_t[4];
data_u = (cmd&0xf0);
data_l = ((cmd<<4)&0xf0);
data_t[0] = data_u|0x0C; //en=1, rs=0
data_t[1] = data_u|0x08; //en=0, rs=0
data_t[2] = data_l|0x0C; //en=1, rs=0
data_t[3] = data_l|0x08; //en=0, rs=0
//HAL_I2C_Master_Transmit (i2c1, SLAVE_ADDRESS_LCD,(uint8_t *) data_t);
I2C_GenerateSTART(I2C1, ENABLE);
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
I2C_Send7bitAddress(I2C1, SLAVE_ADDRESS_LCD, I2C_Direction_Transmitter);
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
I2C_SendData(I2C1,(uint8_t*)data_t);
while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-10 10:39 AM
> I2C_SendData(I2C1,(uint8_t*)data_t);
That won't even compile. Did you try to compile?
I think you need to understand the fundamental difference between (uint8_t) and (uint8_t *). This is a basic C programming concept.