2020-03-19 12:48 AM
Halo,
I am using sensortile and currently trying to be familiar with FP AI Sensing. There is an instruction to enable SENSING1_USE_PRINTF in SENSING1_config.h. I did enable it, however there is an error during compilation, and to solve I need to put SENSING1_USE_PWR_MGNT to 0.
The compilation has no error, however my teraterm COM port still doesnt receive any output from sensortile.
Anybody has tried this before?
Thank you
2020-04-14 06:10 AM
I am facing same issue...Did you make it work is it something to do with 10s delay?
2020-04-14 06:20 AM
I didnt manage to make it work. I did confirm that it is not HW issue since I program other FW demo and the UART works.
So it must be the FW issue or I miss out something on the FW steps.
2020-04-14 06:44 AM
Did you try this initiallization. I will let you if I am able find it out.
2020-04-14 06:46 AM
2020-04-15 10:34 AM
I also tried it is not working for me as well
2020-04-21 10:00 PM
Hello HKart,
Please find this link for the resolution of this issue.