2017-09-17 4:42 PM
Hello,
CubeMX is missing some lines of code, so the FMC will not work with the generated code.
CubeMX Version: 4.22.1
CPU: SMT32F427VG..
First I configured the FMC for my TFT display with the standard libs and all worked fine.
Then I used CubeMX to generate the same code using HAL.
In general the code is correct, but two important things are missing in MX_FMC_Init():
1. at the beginning the FMC clock must be enabled: __HAL_RCC_FMC_CLK_ENABLE();
2. the GPIOs of the FMCs are not initialized as alternate function, so I added:
GPIO_InitTypeDef GPIO_Init_Structure;
GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP; GPIO_Init_Structure.Pull = GPIO_NOPULL; GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH; GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_4 | GPIO_PIN_5 |
GPIO_PIN_7 | GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_14 | GPIO_PIN_15; HAL_GPIO_Init(GPIOD, &GPIO_Init_Structure);GPIO_Init_Structure.Pin = GPIO_PIN_7 | GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 |
GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15; HAL_GPIO_Init(GPIOE, &GPIO_Init_Structure);with this additional code everything works perfectly.
Maybe one of the CubeMX programmers can look at this issue and add this code into the automatic program generator.
Harry
2017-09-18 9:30 AM
Hello
harry4516
,Itested with the same board and CubeMX version (4.1):The
FMC clock is enabled and the
GPIOs are initialized in STM32F4xx_hal_msp.c file.Please, try to share your ioc file to check your issue.
Kind Regards
Imen
2017-09-18 3:26 PM
Hello Imen,
thank you for answering.
How to reproduce the problem:
In CubeMX 4.22.1: New Project, select STM32F427VG, Start Project
Configure: FMC for LCD, A16, 16bit
Configure: RRC enable ext Clock
Generate program. This is all I have done.
If I look into STM32F4xx_hal_msp.c then I see no Clock or GPIO init, only Priority settings.
I have put the files on my server:
ioc-File:
http://www.dj0abr.de/files/fmctest.ioc
complete project as ZIP:
http://www.dj0abr.de/files/fmctest.zip
Kind Regards
Harry