cancel
Showing results for 
Search instead for 
Did you mean: 

Flashing an encrypted Firmware

j_filipe
Associate III

Greetings, 
I am using a STM32U585 MCU and I made a custom made code that implements the DFU protocol. I could successfully flash a firmare through .bin file and set the Option Bytes, set RDP level 1 and go back to RDP level 0. 
What I want to do is to be able to flash an encrypted firmware into the board using my method. So obviously, I can't do it through the STM32CubeProgrammer or STM32TrustedPackageCreator since I don't want to depend from any ST HSM smartcard, so I guess I can't do it with SFI way. Is there any other way to encrypt a firmware file, then upload it to the board and the board itself be capable of decrypt the firmware and run it? 
BTW, I am being using the B-U585I-IOT02A board to make the tests.
Thank you! 

0 REPLIES 0