cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G491KCU3/6 Differences

mccabehm
Senior

I found https://community.st.com/t5/stm32-mcus-products/stm32g491kxu6-don-t-have-exposed-die-pad/m-p/625099#M231656 on differences between STM32G491KCU3 and KCU6. Is junction temperature range the only difference between these parts?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Correct, the last digit, in this case 3 and 6, only indicates the temperature range within which the respective device is guaranteed to function without errors. Apart from the price, there are no other differences.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Correct, the last digit, in this case 3 and 6, only indicates the temperature range within which the respective device is guaranteed to function without errors. Apart from the price, there are no other differences.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.