2015-11-20 4:29 AM
Hello
I need some help to understand my problem. I'm using eeprom emulation V3.1.0 MCD from Application Team and that works fine. When I reboot I get the PGPERR and PGSERR bits set after a while. I placed breakpoints on all functions that program or erase the flash, so I'm sure they are not reached. What else can set these bits ? P.S. I'm working on STM32F407. Regards #flash2015-11-24 6:26 AM
Hello
I found my problem : Some pointer tried to write at address 0 on my STM32F4. It setted PGPERR and PGSERR bits but did not raised a HardFault ... Regards2015-11-25 1:28 AM
Hi,
you mention V3.1.0 for the EEPROM emulation. Is this a new version? I can't find this on the ST website. I still work with 1.0.0 from 2011, for which I needed to integrate the old SPL Flash driver into my Cube HAL based project. Regards, Ralph2015-11-25 5:20 AM
Hi christopher.ralph,
AN3969 with associated firmware (version 1.0.0) has to be used for STM32F40x/41x devices (http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257902
).The version 3.1.0 is the one to be used for STM32101/103 devices (http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF257846
).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.