cancel
Showing results for 
Search instead for 
Did you mean: 

flash memory endurance of STM32F030

jaeshik
Associate
Posted on January 17, 2016 at 03:08

Hi~

I'm under review for EEPROM emulation on STM32F030.

but, I found that flash memory endurance is min 1000 cycle(1K).

Unfortunately, It is short to use in my project.

Do you know why it is shorter than other STM32?

Most of the other STM32 is a flash endurance is min 10K.
1 REPLY 1
Posted on January 17, 2016 at 15:41

Based on the design, process geometry and testing, they have less confidence in the long term performance?

If you really need EEPROM, use one instead of pretending that FLASH is a substitute. Consider if NVRAM is an alternative.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..