Input Capture module in pulse count example
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-15 10:49 PM
Hello all,
In an external pulse count application, is it possible to capture Timer counts at fixed interval using input capture (IC) module while external input (TIM5_CH1) is driving timer time-base (through TI1F_ED).
I've also tried just storing TIM5->CNT at every RTC interrupt, but found some irregular counts. May be this irregularity is for other interrupts (of high priority) with LP Sleep implementations.
I request some advice on how to configure this capture module (if possible on STML151, clock tree attached). I've configured TIM_5 like this:
......... ......... /* Reset the CC1E Bit to configure CC1S bit of CCMR1 Reg */ TIM5->CCER &= (uint16_t)~((uint16_t)TIM_CCER_CC1E); tmpccmr1 = TIM5->CCMR1; tmpccer = TIM5->CCER; /* TIM5 Input CH1 is selected to be connected to IC1. and reset the filter */ tmpccmr1 &= (uint16_t)(((uint16_t)~((uint16_t)TIM_CCMR1_CC1S)) & ((uint16_t)~((uint16_t)TIM_CCMR1_IC1F))); tmpccmr1 |= (uint16_t)(TIM_ICSelection_DirectTI | (uint16_t)(0x00 << (uint16_t)4)); /* IC Rising edge and set the CC1E Bit */ tmpccer &= (uint16_t)~((uint16_t)(TIM_CCER_CC1P | TIM_CCER_CC1NP));/* Write to TIM5 CCMR1 and CCER registers */
TIM5->CCMR1 = tmpccmr1; TIM5->CCER = tmpccer; //Input Trigger source TIM_TS_TI1F_ED: TI1 Edge Detector. TIM_SelectInputTrigger(TIM5, TIM_TS_TI1F_ED); //Slave Mode TIM_SlaveMode_External1: SMS=111 TIM_SelectSlaveMode(TIM5, TIM_SlaveMode_External1); /* TIM5 enable counter */ TIM_Cmd(TIM5, ENABLE);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-16 6:23 AM
You mention ''irregularity'' but neither define the numbers you are seeing, or the frequency of the signal, or expectations.
If you had a 1 Hz pulse you could apply that to CH2 and have it latch CNT into CCR2 You could use another timer, triggering a DMA1 read of CNT, the latency/jitter in that sample point would be smaller than an interrupt.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-16 8:58 AM
Thank you for your kind response.
I've a fixed custom PCB to work with (~MHz input source for Tim5_CH1). I afraid I can't add any external module/input right now. I guess, internal trigger or another timer can't be applied/routed to TI2.
From L151 datasheet, DMA requests can be generated from Tim2-7 peripherals only. As internal clock changes in Run/LP sleep mode, I'm trying to avoid Timer internal clock to initiate DMA transfer. Here, only Tim9-11 has (LSE) independent clock source.
Could you please suggest me an alternative (if any) for this peripheral-memory DMA configuration.
Thank you for your time.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-16 2:38 PM
> I've a fixed custom PCB to work with (~MHz input source for Tim5_CH1). I afraid I can't add any external module/input right now. I guess, internal trigger or another timer can't be applied/routed to TI2.
You have a more substantial problem. The timers' inputs are synchronized, so you have to have a high-speed APB clock running to be able to run the timer from an external clock. See fEXT specification in the Timer characteristics section of datasheet. JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-16 7:12 PM
Thank you JW,
I've founnd, f_EXT is 0 ~ f_TIMxCLK/2.I have a confusion, is it necessary to have fixed processor clock (or APB1 clock) for accurate external pulse count ? If LP_sleep/Run mode toggles, APB1 or TIMxCLK would change.
I've configured for External clock source mode 1 and reference timing diagram is attached for your kind comment.
Thank you ________________ Attachments : External_clock_source_mode_1_Stm32l151.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16X&d=%2Fa%2F0X0000000bic%2F601vhwYWE4CX8yHyqCC0rs7Z1mbbP1v.kxabdBkD.jo&asPdf=false