2010-04-20 12:58 AM
Flash Loader Demonstrator Crash / AN3155
2011-05-17 4:48 AM
For the Write
31 CE 79 [ACK] 20 00 00 00 20 79 [ACK] 0F 00 11 22 33 44 55 66 77 88 99 AA BB CC DD EE FF 0F 79 [ACK] Where 0F^00^11^22^33^44^55^66^77^88^99^AA^BB^CC^DD^EE^FF = 0F and 20^00^00^00 = 202011-05-17 4:48 AM
Hello all,
how can I get the demonstrator source package? I just can find application not, without source code. Thanks2011-05-17 4:48 AM
Thanks damh, thanks clive,
flashing works now. I had an additional error in my length byte. The STM32 expects nr_of_databytes - 1 in the length byte. Carsten2011-05-17 4:48 AM
The two versions I have put the source files in the ''Program Files\ST Micro whatever'' directory where it installed the GUI Flash Loader application.
2011-05-17 4:48 AM
I don't have the software package installed. I searched ST site and I just found the pdf application note, not the software iitself (GUI Flash Loader application). Where can I find this last?
Thanks2011-05-17 4:48 AM
You can find the Flash Loader Demonstrator (serial) or DFUse (usb) on
http://www.st.com/mcu/inchtml-pages-stm32.html when you click on the MCU you are using (i.e. http://www.st.com/mcu/devicedocs-STM32F103RD-110.html) in the section PC-Software. Carsten2011-05-17 4:48 AM
Got it, thanks