cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Bank2 Pages Write / Erase Problem

melihcicek
Associate II
Posted on April 15, 2011 at 14:36

Flash Bank2 Pages Write / Erase Problem

5 REPLIES 5
Posted on May 17, 2011 at 14:31

FLASH_ClearFlag(FLASH_FLAG_BANK2_EOP | FLASH_FLAG_BANK2_PGERR | FLASH_FLAG_BANK2_WRPRTERR);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist II
Posted on May 17, 2011 at 14:31

Cross post: 

http://www.keil.com/forum/18780/

melihcicek
Associate II
Posted on May 17, 2011 at 14:31

Thank you clive1

It works now

I want to ask one more question

I can erase pages using FLASH_ErasePage(addr); but it erase 2K

but if i want to delete only one byte I mean how can i delete only 0x08002000 address  content !!!

Andrew Neil
Evangelist II
Posted on May 17, 2011 at 14:31

''It works now''

 

 

So be sure to update your thread on the Keil forum!

 

Otherwise you will be wasting people's time over there responding to a question that's already been answered.

 

''if i want to delete only one byte I mean how can i delete only 0x08002000 address  content !!!''

You can't!

It is in the nature of all Flash devices - not just the STM32 - that you can only erase whole pages at a time.

Have you read the ST Application Note about using the Flash to simulate EEPROM...?

melihcicek
Associate II
Posted on May 17, 2011 at 14:31

Hi!

it worked but it is with problem.

When i try to erase, it returns FLASH_Timeout but it erase.

FLASH_Status1 = FLASH_EraseAllBank2Pages();

Also when i write data it write but function return FLASH_TIMEOUT

so it writes more slowly (these problems only for bank2)

I didnt understand the problem !!!