2009-08-26 03:24 AM
Firmware Lib problem calc BRR register for usart
2011-05-17 04:21 AM
Hello,
hopefully anyone can help me. I use the STM32F107VCT6 on the STM3210c-Eval board. is it possible that the library function ''USART_Init'' works not correct? I setup the USART 2 and use the lib-function and the Usart-init struct. when I try to get the USART2 work with 9600 baud with the lib-function it doesn’t work. But if I calculate the BRR Register values ''by hand'' it works fine! I tried to get the system clocks with the lib-function ''RCC_GetClocksFreq'' but this function gives strange frequencies! so maybe this function works not correct? here the usart configuration: ----------------------------- void SetUSART(){ /* The following example illustrates how to configure the USART1 */ /* Resets the USART1 registers to their default reset value */ RCC_ClocksTypeDef RCC_ClocksStatus; // for test USART_DeInit(USART2); USART_Cmd(USART2, ENABLE); // Enable USART 2 USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; RCC_GetClocksFreq(&RCC_ClocksStatus); //for test USART_Init(USART2, &USART_InitStructure); // init USART 2 with init structure USART_ITConfig(USART2, USART_IT_RXNE , ENABLE); // Enables the USART2 Receive interrupt USART_ITConfig(USART2, USART_IT_TXE, ENABLE); // Enables the USART2 Transmission Complete interrupt /* Write to USART BRR */ USART2->BRR = 0x146; //20,36d } here the clock configuration: ----------------------------- void SetCLK(){ ErrorStatus HSEStartUpStatus; // RCC = Reset Clock Control /* RCC system reset(for debug purpose) */ RCC_DeInit(); /* Enable HSE (>High speed external clock here: 25Mhz)*/ RCC_HSEConfig(RCC_HSE_ON); // switch to external oscillator /* Disable Internal High Speed oscillator */ RCC_HSICmd(DISABLE); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); // check stable clock source if(HSEStartUpStatus == SUCCESS){ /* HCLK = SYSCLK */ RCC_HCLKConfig(RCC_SYSCLK_Div1); // System Clock /* PCLK2 = HCLK */ RCC_PCLK2Config(RCC_HCLK_Div1); // peripheral clock 2 /* PCLK1 = HCLK/2 */ RCC_PCLK1Config(RCC_HCLK_Div2); // peripheral clock 1 /* Flash 2 wait state */ FLASH_SetLatency(FLASH_Latency_2); /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); /* PLLCLK = 25MHz * 2 = 50 MHz */ RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_2); // PLL clock /* Enable PLL */ RCC_PLLCmd(ENABLE); // enable the pll clock /* Wait till PLL is ready */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET){} // wait until PLL is ready /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);// system clock = PLLCLOCK /* Wait till PLL is used as system clock source */ while(RCC_GetSYSCLKSource() != 0x08){} // wait for ready clock /* Configure HCLK such as HCLK = SYSCLK (AHB prescaler)*/ RCC_HCLKConfig(RCC_SYSCLK_Div1); /* Configure PCLK1 such as PCLK1 = HCLK/16 (APB1 Prescaler)*/ // PCLK1 for: TIM2 and USART2 RCC_PCLK1Config(RCC_HCLK_Div16); } /* Enable GPIO and USART1 clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ALL, ENABLE); /* Enable Timer2..7 clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_ALL, ENABLE); } thanks for any helpnullhere the clock configuration:2011-05-17 04:21 AM
Hi Christoph,
How did you found that your resulting baud is not correct? I mean are you using some debugger or simulator to do that? First ensure that you have modified the oscillator specification as per your hardware #define HSE_Value ((u32)8000000) /* change here in stm32f10x_conf.h */ In case you are using keil simulator, ensure that Xtal specification in Target option is same as HSE_Value. Also, the keil simulator some time misbehaves for the peripheral clock values shown in dialog box. To ensure this doesn't happen, first open, peripherals -> power, reset and clock control window..... close it then open the respective peripheral windows!! :-] Regards, Varun2011-05-17 04:21 AM
thanks Varun,
I use the Ride7 with the Rlink to debug the Evalboard. I can see the clock frequencies in the watchwindow. Thanks for the tip in the *conf.h i forgot... ;-) Now the frequencies are correct. I added the sourcecode files *usart.c and *rcc.c and all works fine. :-D thanks for your help