2007-08-19 8:54 PM
Fault Tolerant I/O
2011-05-17 3:15 AM
In the pin descriptions section of the data sheet (Table 3), each pin is defined as whether it is 5V tolerant (FT). Unfortunately, PB5 (which I hope to use as an open drain output - returned to 5V) is not shown as being FT.
Q. Does the term 'FT' refer to the input or the output function - or both? Q. What would be the best way to ensure this pin is FT? I was thinking along the lines of an N channel FET as per Figure 20 in the UM0426 Evaluation board User Manual Any thoughts? [ This message was edited by: _adrian_ on 25-07-2007 11:47 ]2011-05-17 3:15 AM
Hi _adrian_,
- The 5V tolerant (FT) refers to the input level for the pins... the STM32 pins with FT capability can support 5V as input but can't generate 5V. - The best way to use the PB5 as FT is to add an external level translator... Regards The Lionheart