Posted on May 17, 2011 at 12:21Quote:I see that board is creating some interest :) This is an early prototype where STM32 is driving 128 Segment (Quadruplex drive) Glass through GPIOs STOne-32Any more details on this, as it looks as if I may be doin...
Posted on May 17, 2011 at 12:19I'm just wondering - should Boot 1 be connected directly to ground as it doubles as Port B-2? What happens if you remove the pull up resistor R48, and connect to ground via a suitable resistor?
Posted on May 17, 2011 at 12:16Here is an update for any other soul struggling with this. I think we have a Rev.A version - if that is what the 'A' represents in the bottom right hand corner of the chip? We are booting from User Flash Memory, which ...
Posted on May 17, 2011 at 12:16We are having problems with the POR function on an STM32F103C8T6. Scoping the reset signal on pin 7, shows a suitable reset signal on power up - but the programme does not run. Tacking an RC network onto the reset pin ...