cancel
Showing results for 
Search instead for 
Did you mean: 

Fault/error when accessing data on internal flash memory STM32H753

GMiki.1
Associate

Hi,

We're storing some device configuration on last sector(7) at BANK2 inside internal flash memory. Sometimes device goes into state where part of this this sector is not readable by our code(generates fault) also this sector is not readable by cubeprogrammer and only solution to make our device work again(make unreadable part readable again) is to mass erase chip.

What could be causing such issue where we cannot read only part of flash memory? How can we check why such region is unreadable?

Some more details:

  • We are always erasing whole sector when we need to change something in config structure and then we reflash it.
  • Data we're storing there is around 1700 bytes currently
  • This happens pretty much randomly and there is no easy way to reproduce it

6 REPLIES 6
TDK
Super User

I would start by looking at the detail of the fault (hard fault?) to find the source of the issue.

If you feel a post has answered your question, please click "Accept as Solution".
GMiki.1
Associate

We know exactly what's causing fault. We are trying to read from certain address from flash memory(in valid range, not protected by anything).

We tracked down the issue and it seems like problem with timings. What we noticed is that after successfully calling "HAL_FLASH_Program()" and restarting device right after we experience corrupted/damaged flash regions. Shouldn't this function ensure that it is safe to turn off device right after it returns? Adding short delay after programming seems to be solving the issue?

Mike1992
Associate III

Hi, were you able to solve this problem? I encountered the same problem and don’t understand how to solve it

Pavel A.
Super User

 Sometimes device goes into state where part of this this sector is not readable by our code(generates fault) 

This can occur as result of programming error (for whatever reason) so access to affected flash area triggers ECC errors. This can be cured by erasing the sector properly. This should reset the ECC. If this won't help, erase the whole bank.

Now, why programming errors can occur... For one, because of the "parallelism" parameter too large for available power. Try lesser (slower) values.

 

 

Mike1992_0-1741942618352.pngMike1992_1-1741942648084.png

Thank you, it helped me to clearly indicate the beginning and end of the memory address and setting 2 ways ICACHE; when setting DIRECT MAPPED CACHE, saving occurred with an error


@Mike1992 wrote:

Mike1992_0-1741942618352.pngMike1992_1-1741942648084.png

Thank you, it helped me to clearly indicate the beginning and end of the memory address and setting 2 ways ICACHE; when setting DIRECT MAPPED CACHE, saving occurred with an error


That's not a STM32H7 product but another MCU part number (maybe H5). If you have an issue please open a new thread an give the part number you are using.

Thanks.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.