2022-04-27 4:46 AM
Hello,
I use STM32F407 MCU and when debugging with Attolic True studio v 9.3.0 I SOMETIMES got following error:
Failure at line 13 in Target software startup scripts
Error finishing flash operation. I attach linker and startup files.
Any help will be appreciated it is really annoying!
Thank you
PS: I see that I am not only one with this problem
2022-04-27 4:54 AM
Atollic Truestudio is frozen at 9.3.0, no longer available and supported and and has been replaced by the free STM32CubeIDE, which can also import projects from Atollic. Maybe this is a way forward for you?
Regards
/Peter