2017-10-28 8:37 AM
Hi ladies, guys,
I am currently working on a project, so I am getting used to work with SMT32 MCUs and more particularly with STM32F411RE. I have built a C program just to blink the led user, in order to reduce flash and RAM as much as possible than the program bed gives us, with a lot of functions, libraries, that we don't use at all.
However, when I flash it on my board, that does not work but the firmware given by bed works so my code is wrong. But I am working on it for many hours and I need some advice and another point of view. Could you tell me what is wrong ?
So here it is :
&sharpinclude 'stm32f4xx.h'
int main() {
/* HSI -> SYSCLK */ RCC->CR |= (1u << 0) ; /* bit 0 at 1 to select HSI */ RCC->CFGR = RCC->CFGR & 0xFFFFFFFC ; /* HSI == SYSCLK */ RCC->PLLCFGR = RCC->PLLCFGR & 0xFFBFFFFF ; /* bit 22 a 0 (2MHz mini) */ RCC->PLLCFGR = RCC->PLLCFGR | 0x00000F0A ; /* 96 MHz (16*60/10) */ RCC->PLLCFGR = RCC->PLLCFGR | 0x02000000 ; /* 48 MHz (96/2) */ RCC->CR = RCC->CR & 0xFFFCFFFF ; /* 48 MHz */ RCC->CR = RCC->CR | 0x02000000 ; /* 48 MHz */ /* PUSH-PULL OUTPUT for GPIOA and PA5 for LED user */ RCC->AHB1ENR |= (1u << 0) ; /* peripheral clock enabled (bit 0 GPIOEN) */ GPIOA->MODER |= (1u << 10) ; /* byte 10 set to 1 */ GPIOA->OTYPER &= ~(1u << 5) ; /* byte 5 put to 0 for output push pull */ /* Configuration of the timer */ RCC->APB1ENR |= (1u << 0) ; /* Enable clock TIM2 (BIT 0 register APB1ENR) */ TIM2->ARR = 6855 ;/*Autoreaload
*/
TIM2->PSC = 10000 ;/* Prescaler
*/
TIM2->DIER |= (1u << 0) ; ; /* Enable interrupt for tim2 */ /* Autorisation interruption */ NVIC->ISER[0] |= (1u << 28); /* Enable interrupt 28 ofr TIM2 */ NVIC->IP[28] = NVIC->IP[28] | (7 << 4); /* Priorit� (7) */ SYSCFG->EXTICR[2] &= 0xFFFFFF0F ; EXTI->IMR |= ( 1u << 5 ) ; /* Masque interruption desactivee EXTI_IMR register */ /* Lancement du timer */ TIM2->CR1 |= (1u << 0) ; /* Counter is on */ while(1) { } return 0 ; }void TIM2_IRQHandler(void){
/* LED on or off */ TIM2->SR &= ~( 1u << 0 ) ; /* UIF puts at 0 */ GPIOA->ODR = GPIOA->ODR ^ (1u << 5);}Thanks a lot !
Best !
#incomplete-code2017-10-28 8:59 AM
Try using a debugger and breaking the problem down.
For example test the XORing of PA5 in the loop, and step through check to see the line go high/low.
Review the TIM/RCC settings the debugger's peripheral view.
The RCC code seem to ignore selection and waiting phases for PLL and clock sources.
2017-10-28 11:22 AM
Thank you very much Clive for your fast response.
Indeed, I tried it, to turn it on and off again and again in my loop, but that does not work as well...
I also wanted to run my program step by step, watching at the registers of my MCU but I got a MAC OS X, and I do not know which software I must install to do it. Step by step will permit me to detect my errors, and correct them.
Do you know how I could do that ?
Thanks !
2017-10-28 2:00 PM
I'm a Windows + Keil guy, so don't have much of an opinion on OSX based tools. I believe Rowley has an OSX offering, and I liked their PC tools.