2016-01-15 09:35 AM
NUCLEO-F746ZG
http://www.st.com/web/en/catalog/tools/FM116/CL1620/SC959/SS1532/LN1847/PF262631
NUCLEO-F446ZEhttp://www.st.com/web/en/catalog/tools/FM116/CL1620/SC959/SS1532/LN1847/PF262632
Nucleo-144 will be with microcontrollers:STM32F207ZGT6STM32F303ZET6STM32F429ZIT6STM32F446ZET6STM32F746ZGT6Provides Ethernet connectivitySolved! Go to Solution.
2016-03-21 01:06 PM
The picture for the F446 model is a bit deceptive, it doesn't actually have Ethernet support.
Currently I have some F446, F429 and F746 Nucleo-144's to play with.Here I wired up a GSM Modem Shield, hooking up a 7V DC supply to VIN to power both the modem and Nucleo.http://www.janus-rc.com/JanusArduinoShield.html
2016-03-21 01:06 PM
The picture for the F446 model is a bit deceptive, it doesn't actually have Ethernet support.
Currently I have some F446, F429 and F746 Nucleo-144's to play with.Here I wired up a GSM Modem Shield, hooking up a 7V DC supply to VIN to power both the modem and Nucleo.http://www.janus-rc.com/JanusArduinoShield.html