cancel
Showing results for 
Search instead for 
Did you mean: 

Any easy way to tell if LSE lock is lost while running: STM32F205

Taylor.Sean
Associate II
Posted on March 21, 2016 at 17:25

We have a batch of boards in the field where the LSE crystal may be marginal and I'm wondering if there's a way to check for the LSE losing lock after initially being locked.  That is, if on initial clock setup I get a positive response from RCC_GetFlagStatus(RCC_FLAG_LSERDY), but later the LSE stops.

I've looked at the RCC_BDCR register and it doesn't seem to change, even if I short out the crystal, but I do see the RTC stop advancing.

So is my only option to check for the RTC stopping advancing and use that to flag a problem ?   Thanks in advance
7 REPLIES 7
waclawek.jan
Super User
Posted on March 21, 2016 at 17:45

> I've looked at the RCC_BDCR register and it doesn't seem to change, even if I short out the crystal, but I do see the RTC stop advancing.

Yes, unfortunately LSE_RDY flag does not seem to reflect the true state of LSE, serving only as a startup indicator. I guess it's just an output from a saturated fixed-count counter fed by LSE.

Some newer STM32 models (e.g. 'L0, I did not check elsewhere) feature a LSE-CSS, but not the 'F2/'F4. You might perhaps want to check out the 'L4.

RTC output event may be fed into TIM5_CH4, see TIM5_OR, but I don't know exactly could that be used for any automatism to check LSE running.

JW

jpeacock
Associate III
Posted on March 21, 2016 at 17:55

If you use the SysTick timer as a timebase, for example in an RTOS, and you generate a 1 second t interrupt from the RTC, then if you get 2 seconds worth of SysTicks but no RTC  you can conclude the LSE failed.

I also reset the IWDG from the 1 second RTC since an LSE failure is a fatal event in my applications.  After a reset if you see the IWDG as the source you know the RTC isn't working and can fall back to the LSI as a workaround.
Taylor.Sean
Associate II
Posted on March 21, 2016 at 19:26

Thanks guys.   I'll use the SysTick interrupt to monitor the RTC and restart it on the LSI if I notice a loss of ticking.   That will suffice for almost all functionality.

Posted on March 21, 2016 at 20:30

RTC output event may be fed into TIM5_CH4, see TIM5_OR, but I don't know exactly could that be used for any automatism to check LSE running.

You can use it to measure the period, or up to 8 periods, of the LSI, or LSE. In a 1ms ticker, you'd expect this timestamp (in TIM5->CCR4) to precess.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on March 21, 2016 at 22:11

By ''automatism'' I meant ''no stinkin' software-checking-periodically, just interrupt me when the clock stops''. Should that channel be CH1 or CH2, I'd tie it to the slave controller and reset the timer from RTC; then set another channel to interrupt just beyond the one second mark. Maybe something similar could be accomplished by employing a DMA triggered by CH4, writing a well-chosen constant to some of the timer's registers.

JW

TanmayKhalas
Associate

So How do we detect that LSE is Working or not?

 

The OP said, "I do see the RTC stop advancing" - so use that?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.