2012-07-05 5:42 AM
2012-07-05 6:22 AM
Got some real issues with your while() loops there. (hint: missing semicolons)
SPI1 references mixed in. I might attack this something like this, working from memory not tested :int main(void)
{ char Received_From_device[500] = ''''; // Maximum data from device of 500 bytes //char character[10] = ''''; char ETX_character; int i,a,lazy_timeout_counter,lazy_timeout_max,tmp,adc_value; char c; RCC_Configuration(); GPIO_Configuration(); SPI2_Configuration(); //SPI configure USART1_Configuration(); GPIO_SetBits(GPIOB, GPIO_Pin_12); //set Chip Select HIGH for SPI while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty USART_SendData(USART1, 0x49); // Send 'I' while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 0x42); // Send 'B' SPI_Loop: Delay(1000); //1second delay //goto Jump2Here; //Select CH0 of LTC2492 GPIO_ResetBits(GPIOB, GPIO_Pin_12); // Assert -CS Delay_us(10); // overkill // You need semicolons after the whiles otherwise they repeat the next statement while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == 0); //wait for transmit buffer to be empty, should be SPI_I2S_ReceiveData(SPI2); // Clear RXNE SPI_I2S_SendData(SPI2, LTC_Internal_Temperature_select); //LTC_Internal_Temperature_select while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == 0); //wait for transmit buffer to not be empty (ie data loaded in) SPI_I2S_SendData(SPI2, 0); // Fill for 32-bits, remaining 16-bits in holding buffer while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == 0); // wait for last bit to be sent SPI_I2S_ReceiveData(SPI2); // Clear RXNE, first word while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == 0); // wait for last bit to be sent SPI_I2S_ReceiveData(SPI2); // Clear RXNE, second word Delay_us(10); GPIO_SetBits(GPIOB, GPIO_Pin_12); // Release -CS Delay(1000); //1second delay //await result readable via SPI and read in result via SPI two 16bit reads over SPI GPIO_ResetBits(GPIOB, GPIO_Pin_12); // Assert -CS Delay_us(10); // overkill while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == 0); // should be empty SPI_I2S_ReceiveData(SPI2); // clear RXNE SPI_I2S_SendData(SPI2, LTC_Internal_Temperature_select); // send command word while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == 0); //wait for transmit buffer to not be empty (ie data loaded in) SPI_I2S_SendData(SPI2, 0); // Fill for 32-bits, remaining 16-bits in holding buffer while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == 0); tmp = SPI_I2S_ReceiveData(SPI2); // read word from receive buffer, high order 16-bits adc_value = tmp * 65536; while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == 0); // wait until receive buffer is not empty tmp = SPI_I2S_ReceiveData(SPI2); // read word from receive buffer, low order 16-bits adc_value = adc_value + tmp; Delay_us(10); GPIO_SetBits(GPIOB, GPIO_Pin_12); // Release -CS Jump2Here: //send result via RS232 while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 0x43); // Send 'C' while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 0x48); // Send 'H' while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 0x30); // Send '0' while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, 0x3A); // Send ':' // Sends as binary, not ascii //adc_value = 1234567890; while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, ((adc_value >> 24) & 0xFF)); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, ((adc_value >> 16) & 0xFF)); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, ((adc_value >> 8) & 0xFF)); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData(USART1, ((adc_value >> 0) & 0xFF)); //goto SPI_Loop; while (1); }2012-07-05 6:35 AM
Thanks Clive, sloppy with my ;s
I have connected up the scope and MISO of LTC2492 goes up and down when not connected to SMT32, but not when connected. This suggests that MISO of the STM32 is configured as an output (PB14). How do I fix that?2012-07-05 6:52 AM
Looking at the code I tried adding in a line at the end of the SPI_Configuration routine that reads:
GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); This seems to have worked. Could a similar line for PB12 fix the Chip Select? I might try that. My code is pretty rough here2012-07-05 7:25 AM
Yeah, just noticed the AF Config as I read through your response
GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); Yes, you would need to mux the pin to the AF device, which also controls the pin directions, so deals with 1-wire or Master/Slave settings, etc. I understand the roughness issue, having mashed out similar code myself trying to make sense of things, and try a couple of avenues. Added or missing semicolons on whiles being particularly easy to overlook.2012-07-05 8:08 AM
I'll try that with NSS when I get the chance. Lots of people seem to have trouble with NSS and bit bashing seems to often be the solution people go for. Would be nice to have a better solution though.
2012-07-05 8:38 AM
Well I have tried it and NSS is still a mystery to me. I added the following line to the SPI_Configuration routine:
GPIO_PinAFConfig(GPIOB, GPIO_PinSource12, GPIO_AF_SPI2);I added GPIO_Pin_12 to the GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; line I then attempted to use SPI_Cmd(SPI2, DISABLE); and SPI_Cmd(SPI2, ENABLE); to control NSS (CS_bar HIGH and LOW respectively) but PB12 doesn't move from being permanently LOW. I can see the SPI clock (PB13) float when the SPI is disabled. If I change SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; to SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; then it stalls on the first while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == 0) line. understanding how to use NSS properly would make the code a lot cleaner and more intuative.
2013-03-18 5:05 PM
Philosophy ON
when I see something like this I just cringe!GPIO_SetBits(GPIOB, GPIO_Pin_12); // Release -CS
and thanks clive1 for adding the commentEmbedded developers should read ''Clean Code''GPIO_SetBits(GPIOB, GPIO_Pin_12);
is completely un-maintainable. Who knows that it it the chip select? Only the person who is married to the code. Suppose Hardware changes the pin? Then you have to find all the instances throughout the code and change them all (hopefully).My goal is to write code that is self documenting code so that I do not write comments (which are often wrong anyway). So that I can give this code to junior engineers and they can learn and maintain it.Philosophy OFF2013-03-18 5:29 PM
Yeah, would always prefer code to be understandable even if comments were removed.
You might find this an entertaining example[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/f407%20board%20with%20examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx¤tviews=65]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Discovery%2ff407%20board%20with%20examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FAllItems.aspx¤tviews=652013-03-19 1:43 PM
more magic numbers than I have ever seen before. :)
Bypass CMSIS?And what happens when a peripheral lib is updated because of some silicon issue?totally un-maintainable. And this is ''for students''? (if the translation is correct)