['F446 documentation] SPDIF-Rx input pins naming/numbering mismatch between DS and RM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-17 4:29 PM
In STM32F446xC/E DS rev.6, Table 10. STM32F446xx pin and ball descriptions, SPDIF-Rx input pins are named SPDIFRX_IN0, SPDIFRX_IN1, SPDIFRX_IN2, SPDIFRX_IN3.
In the same DS, Table 11. Alternate function, the same pins are named SPDIF_RX0, SPDIF_RX1, SPDIF_RX2, SPDIF_RX3.
In RM0390 rev.3, in 27.3 SPDIFRX functional description, these pins are referred to as SPDIFRX_IN[4:1] and in Figure 337. SPDIFRX block diagram as SPDIFRX_IN[1], SPDIFRX_IN[2], ..., SPDIFRX_IN[n] where n=4.
In the same RM, 27.5.1 Control register (SPDIFRX_CR), INSEL bitfield description, these pins are named SPDIFRX_IN1, SPDIFRX_IN2, SPDIFRX_IN3, and SPDIFRX_IN4.
There are still no bitfield values defined in the CMSIS-mandated device header, so I can't comment on that (but wrote this deliberately to remind once again of my request for these values). I don't care about Cube and kin.
In other words, regardless of 3 different naming scheme, the DS numbers pins from 0, whereas RM from 1. That's very, very confusing.
Please, unify the pins names and numbering.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-12-28 7:32 AM
Hello Jan,
Sorry for the delay to answer you.
Your feedback regarding SPDIFRX pins naming/numbering is passed internally and the pins names and numbering will be corrected for all datasheets including SPDIFRX:
SPDIFRXx_INx with SPDIFRX input (x=1,2,3,4).
Thank you for your contribution and Happy New year.
Kind Regards,
Imen
Thanks
Imen