F103 ADC DMA - help ! a question
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 8:55 AM
hello dear forum,
I want use ADC + DMA with F103
I want start ADC conversion with external input and want
ADC convert 50 samples and stop until next start
however with every start ADC measures one single sample and put it in the target array
with incrementing the target array adres
please advice
thank you
my code
--------------------------------------------------------
void init_adc1(void)
{
// ADC_InitTypeDef ADC_InitStructure;
GPIO_InitStructure.GPIO_Pin = /*GPIO_Pin_4|*/GPIO_Pin_5 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOC, &GPIO_InitStructure);
// RCC_ADCCLKConfig(RCC_PCLK2_Div2);
ADC_DeInit(ADC1);
ADC_InitStructure.ADC_ScanConvMode = ENABLE; // tarama modu a�?k
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 2; //
ADC_Init(ADC1, &ADC_InitStructure);
adc_channel_config();
ADC_DMACmd(ADC1,ENABLE);
ADC_Cmd(ADC1, ENABLE);
ADC_ResetCalibration(ADC1);
while(ADC_GetResetCalibrationStatus(ADC1));
ADC_StartCalibration(ADC1);
while(ADC_GetCalibrationStatus(ADC1));
}
void ADC1_DMAConfig(void){
DMA_InitTypeDef DMA_InitStructure;
DMA_Cmd(DMA1_Channel1,DISABLE);
DMA_DeInit ( DMA1_Channel1);
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)0x4001244C; // ADC->DR Adresi
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) ADC_ValArray; // hedef adresimiz
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; // ADC kaynak. Veri y�n� ADC -> Haf?za
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; // ADC adresi sabit kalacak
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; // Her de?er al?nd???na memory adresi 1 art?r?lacak
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; // Kaynaktan al?nacak veri 16 bit
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; // Hedef b�y�kl�?� 16 bit
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; //veri al?nd?ktan sonra ba?a d�n�lecek.
DMA_InitStructure.DMA_Priority = DMA_Priority_High ; // Kanal �nceli?i y�ksek. ( bu bize kalm??)
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; // haf?zadan haf?zaya transfer kapal?.
DMA_InitStructure.DMA_BufferSize = 100; //
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);
DMA_Cmd(DMA1_Channel1,ENABLE);
}
if (GPIOB->IDR&GPIO_Pin_9) RAM[0]=0;else RAM[0]=1;
if(RAM[0]&&!RAM[20])ADC_ExternalTrigConvCmd(ADC1, ENABLE);
RAM[20]=RAM[0];
#dma #f103 #adc- Labels:
-
ADC
-
DMA
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 9:49 AM
There is probably a way of using TIM1 or TIM8 in a One Pulse - Repetition Count mode.
Have the ADC trigger via TIM.
Trigger the TIM to capture 50 events.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-21 5:16 AM
hello thanks for answering
I searched Google for a F103 + TIM triggered + ADC + DMA example but couldnot find it
also I couldnot get the SP Library example working
can anybody share a working SPL code please
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-21 6:34 AM
I got it working - thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-21 7:56 AM
I got it working but following ;
It ADConvert only 1 time for every trigger
but I set the DMA buffer size to 50 for single channel
how can I make it ADConvert a sequence of samples for each trigger ?
thank you
my code
--------------------
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)0x4001244C;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) ADC_ValArray; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High ; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_InitStructure.DMA_BufferSize = 100;----
ADC_InitStructure.ADC_ScanConvMode = DISABLE ;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T2_CC2; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 2; ADC_Init(ADC1, &ADC_InitStructure)--------------------
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-22 4:01 AM
noone has any idea ?