cancel
Showing results for 
Search instead for 
Did you mean: 

External RAM on STM32H743IIT6

GGowi.1
Associate II

I am trying to set up FMC to work with external RAM. The code compiles and works with KEIL, but I am trying to make it work with STM32CubeIDE. The code compiles and runs, but the RAM is not initialized. I copied all of the code, including the .ioc file, and used it but it won't enable the RAM.

I have a temporary license for KEIL and I have confirmed that the memory and the code work by compiling and debugging in KEIL and accessing the RAM in the code and in the debugger.

Any thoughts or ideas? I need this external ram so I can continue to port TouchGFX to my board for a research project.

Thanks

This discussion is locked. Please start a new topic to ask your question.
18 REPLIES 18

I thought that the same code would work, too. I'll do some more debugging and make sure that CubeMX didn't change anything when it imported the project.

PMath.4
Senior III

I'm using the Waveshare board with STM32CubeIDE. I'll attach the various bits of relevant code. Willl take more than 1 post due to size limits on the forum

IN main.c start the clocks including the FMC clock

void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
  /** Supply configuration update enable 
  */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
  /** Configure the main internal regulator output voltage 
  */
  if(HAL_GetREVID()==0x1003)__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
  else __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
 
  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
  /** Configure LSE Drive Capability 
  */
  __HAL_RCC_BKPRAM_CLK_ENABLE();
  HAL_PWREx_EnableBkUpReg();
  HAL_PWR_EnableBkUpAccess();
  /** Macro to configure the PLL clock source 
  */
  __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI
                              |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON  ;
  RCC_OscInitStruct.LSEState = RCC_LSE_ON;
  RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 1;
  RCC_OscInitStruct.PLL.PLLN = (MAINCLOCKSPEED>>2);
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 20;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
  RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    SystemError=1;Error_Handler();
  }
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, (HAL_GetREVID()==0x1003 ? FLASH_LATENCY_2:FLASH_LATENCY_4)) != HAL_OK)
  {
    SystemError=1;Error_Handler();
  }
  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_LTDC
                              |RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_UART4
                              |RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_RNG
                              |RCC_PERIPHCLK_SPI3|RCC_PERIPHCLK_SPI1
                              |RCC_PERIPHCLK_SPI2|RCC_PERIPHCLK_I2C2
                              |RCC_PERIPHCLK_ADC|RCC_PERIPHCLK_I2C1
                              |RCC_PERIPHCLK_I2C4|RCC_PERIPHCLK_USB
                              |RCC_PERIPHCLK_FMC;
  PeriphClkInitStruct.PLL2.PLL2M = 1;
  if(HAL_GetREVID()==0x1003){
	  PeriphClkInitStruct.PLL2.PLL2N = 100;
	  PeriphClkInitStruct.PLL2.PLL2P = 16;
	  PeriphClkInitStruct.PLL2.PLL2Q = 16;
	  PeriphClkInitStruct.PLL2.PLL2R = 4;
  } else {
	  PeriphClkInitStruct.PLL2.PLL2N = 120;
	  PeriphClkInitStruct.PLL2.PLL2P = 20;
	  PeriphClkInitStruct.PLL2.PLL2Q = 20;
	  PeriphClkInitStruct.PLL2.PLL2R = 5;
  }
  PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
  PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
  PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
  PeriphClkInitStruct.PLL3.PLL3M = 1;
  if(HAL_GetREVID()==0x1003){
	  PeriphClkInitStruct.PLL3.PLL3N = 100;
	  PeriphClkInitStruct.PLL3.PLL3P = 20;
	  PeriphClkInitStruct.PLL3.PLL3Q = 20;
	  PeriphClkInitStruct.PLL3.PLL3R = 20;
  } else {
	  PeriphClkInitStruct.PLL3.PLL3N = 120;
	  PeriphClkInitStruct.PLL3.PLL3P = 24;
	  PeriphClkInitStruct.PLL3.PLL3Q = 24;
	  PeriphClkInitStruct.PLL3.PLL3R = 24;
  }
  PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_3;
  PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL3VCOWIDE;
  PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
  PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_PLL2;
  PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL2;
  PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_PLL2;
  PeriphClkInitStruct.Usart16ClockSelection = RCC_USART16CLKSOURCE_PLL2;
  PeriphClkInitStruct.RngClockSelection = RCC_RNGCLKSOURCE_HSI48;
  PeriphClkInitStruct.I2c123ClockSelection = RCC_I2C123CLKSOURCE_HSI;
  PeriphClkInitStruct.UsbClockSelection = (HAL_GetREVID()==0x1003 ? RCC_USBCLKSOURCE_HSI48:RCC_USBCLKSOURCE_PLL);
  PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_HSI;
  PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
  PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    SystemError=1;Error_Handler();
  }
  HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_1);
  /** Enable USB Voltage detector 
  */
  HAL_PWREx_EnableUSBVoltageDetector();
}

PMath.4
Senior III

Setup FMC and SDRAM

void RAMSETUP(void){
	  /*##-1- Configure the SDRAM device #########################################*/
	  /* SDRAM device configuration */
	  hsdram.Instance = FMC_SDRAM_DEVICE;
 
	    /* Timing configuration for 100Mhz as SDRAM clock frequency (System clock is up to 200Mhz) */
	  SDRAM_Timing.LoadToActiveDelay    = 2;
	  SDRAM_Timing.ExitSelfRefreshDelay = 7;
	  SDRAM_Timing.SelfRefreshTime      = 4;
	  SDRAM_Timing.RowCycleDelay        = 7;
	  SDRAM_Timing.WriteRecoveryTime    = 2;
	  SDRAM_Timing.RPDelay              = 2;
	  SDRAM_Timing.RCDDelay             = 2;
 
	  hsdram.Init.SDBank             = FMC_SDRAM_BANK2;
	  hsdram.Init.ColumnBitsNumber   = FMC_SDRAM_COLUMN_BITS_NUM_8;
	  hsdram.Init.RowBitsNumber      = FMC_SDRAM_ROW_BITS_NUM_12;
	  hsdram.Init.MemoryDataWidth    = FMC_SDRAM_MEM_BUS_WIDTH_16;
	  hsdram.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
	  hsdram.Init.CASLatency         = FMC_SDRAM_CAS_LATENCY_3;
	  hsdram.Init.WriteProtection    = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
	  hsdram.Init.SDClockPeriod      = FMC_SDRAM_CLOCK_PERIOD_2;
	  hsdram.Init.ReadBurst          = FMC_SDRAM_RBURST_ENABLE;
	  hsdram.Init.ReadPipeDelay      = FMC_SDRAM_RPIPE_DELAY_1;
 
	  /* Initialize the SDRAM controller */
	  if(HAL_SDRAM_Init(&hsdram, &SDRAM_Timing) != HAL_OK)
	  {
	    /* Initialization Error */
	    SystemError=1;Error_Handler();
	  }
 
	  /* Program the SDRAM external device */
	  SDRAM_Initialization_Sequence(&hsdram, &command);
 
}

PMath.4
Senior III

Configure the pins

static uint32_t FMC_Initialized = 0;
 
static void HAL_FMC_MspInit(void){
  /* USER CODE BEGIN FMC_MspInit 0 */
 
  /* USER CODE END FMC_MspInit 0 */
  GPIO_InitTypeDef GPIO_InitStruct ={0};
  if (FMC_Initialized) {
    return;
  }
  FMC_Initialized = 1;
 
  /* Peripheral clock enable */
  __HAL_RCC_FMC_CLK_ENABLE();
  
  /** FMC GPIO Configuration  
  PF0   ------> FMC_A0
  PF1   ------> FMC_A1
  PF2   ------> FMC_A2
  PF3   ------> FMC_A3
  PF4   ------> FMC_A4
  PF5   ------> FMC_A5
  PH5   ------> FMC_SDNWE
  PF11   ------> FMC_SDNRAS
  PF12   ------> FMC_A6
  PF13   ------> FMC_A7
  PF14   ------> FMC_A8
  PF15   ------> FMC_A9
  PG0   ------> FMC_A10
  PG1   ------> FMC_A11
  PE7   ------> FMC_D4
  PE8   ------> FMC_D5
  PE9   ------> FMC_D6
  PE10   ------> FMC_D7
  PE11   ------> FMC_D8
  PE12   ------> FMC_D9
  PE13   ------> FMC_D10
  PE14   ------> FMC_D11
  PE15   ------> FMC_D12
  PH6   ------> FMC_SDNE1
  PH7   ------> FMC_SDCKE1
  PD8   ------> FMC_D13
  PD9   ------> FMC_D14
  PD10   ------> FMC_D15
  PD14   ------> FMC_D0
  PD15   ------> FMC_D1
  PG4   ------> FMC_BA0
  PG5   ------> FMC_BA1
  PG8   ------> FMC_SDCLK
  PD0   ------> FMC_D2
  PD1   ------> FMC_D3
  PG15   ------> FMC_SDNCAS
  PE0   ------> FMC_NBL0
  PE1   ------> FMC_NBL1
  */
  GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 
                          |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_11|GPIO_PIN_12 
                          |GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
  HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
  GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
  HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
 
  GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5 
                          |GPIO_PIN_8|GPIO_PIN_15;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
  HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
  GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10 
                          |GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14 
                          |GPIO_PIN_15|GPIO_PIN_0|GPIO_PIN_1;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
  HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
  GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_14 
                          |GPIO_PIN_15|GPIO_PIN_0|GPIO_PIN_1;
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
  /* USER CODE BEGIN FMC_MspInit 1 */
 
  /* USER CODE END FMC_MspInit 1 */
}
 
void HAL_SDRAM_MspInit(SDRAM_HandleTypeDef* hsdram){
  /* USER CODE BEGIN SDRAM_MspInit 0 */
 
  /* USER CODE END SDRAM_MspInit 0 */
  HAL_FMC_MspInit();
  /* USER CODE BEGIN SDRAM_MspInit 1 */
 
  /* USER CODE END SDRAM_MspInit 1 */
}
 

PMath.4
Senior III

Main code startup

  SystemClock_Config();
RAMSETUP();
FMC_Bank1_R->BTCR[1] = 0x000030D2;
HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAMB2);

PMath.4
Senior III

Set up refresh

static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram, FMC_SDRAM_CommandTypeDef *Command)
{
  __IO uint32_t tmpmrd =0;
  /* Step 1:  Configure a clock configuration enable command */
  Command->CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
  Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;;
  Command->AutoRefreshNumber = 1;
  Command->ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, Command, SDRAM_TIMEOUT);
 
  /* Step 2: Insert 100 us minimum delay */
  /* Inserted delay is equal to 1 ms due to systick time base unit (ms) */
  HAL_Delay(1);
 
  /* Step 3: Configure a PALL (precharge all) command */
  Command->CommandMode = FMC_SDRAM_CMD_PALL;
  Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
  Command->AutoRefreshNumber = 1;
  Command->ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, Command, SDRAM_TIMEOUT);
 
  /* Step 4 : Configure a Auto-Refresh command */
  Command->CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
  Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
  Command->AutoRefreshNumber = 8;
  Command->ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, Command, SDRAM_TIMEOUT);
 
  /* Step 5: Program the external memory mode register */
  tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_1          |
                     SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL   |
                     SDRAM_MODEREG_CAS_LATENCY_3           |
                     SDRAM_MODEREG_OPERATING_MODE_STANDARD |
                     SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;
 
  Command->CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
  Command->CommandTarget = FMC_SDRAM_CMD_TARGET_BANK2;
  Command->AutoRefreshNumber = 1;
  Command->ModeRegisterDefinition = tmpmrd;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, Command, SDRAM_TIMEOUT);
 
  /* Step 6: Set the refresh rate counter */
  /* Set the device refresh rate */
  HAL_SDRAM_ProgramRefreshRate(hsdram, REFRESH_COUNT);
 
}

Can you attach your .ioc file? It looks like most of this code is autogenerated by CubeMX. I'm trying to figure out which settings to change so I don't have to go in and change the files manually each time.

Where are you getting the variable command?

OK - this all works... wow. Thank you so much!

I just have to find a way to keep CubeMX from overwriting the code each time I rebuild so I can add the call to SDRAM_Initialization_Sequence.