2014-07-30 5:14 AM
I am working on a project on the stm32 eval2 board that requires about 600 kB of RAM. Do I need to add external memory to the FMC bus? Or is all the memory I need already provided with the board. I do not understand this very well, I don�t think, so any help would be appreciated. Also I am using keil v5 and c++.
#eval #stm32 #keil #c++2014-07-30 7:01 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/RAM%20in%20stm32%20eval%20board&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=32]Previous Thread
Are you a PC programmer? What kind of computer/engineering skills are you bringing to the party? Trying to gauge here what knowledge we can leverage when explaining things in a manner you will most easily grasp. Do you have any colleagues with embedded experience? Do we agree we're talking about thehttp://www.st.com/web/en/catalog/tools/PF259094
board? Have you reviewed the User Manual and Schematic for the design? Have you observed the chips on the board, that are represented to be memory chips? The code to enable the external memory bus (FMC/FSMC), and the chips attached to it, will generally be found in the system_stm32f4xx.c file tailored to the board, and the examples for it. Have you look at that?2014-07-30 7:14 AM
2014-07-31 2:42 AM
I do not have much experience and I do not have any colleagues with embedded experience unfortunately.
I have looked at the schematic and the memory map, but I am having a hard time figuring out where to initialize the RAM.2014-07-31 4:57 AM
From what I am understanding from the memory map (attached), I need to add some external RAM to meet my needs because all of the memory set aside for RAM is being used.
________________ Attachments : ScreenHunter_001.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I11P&d=%2Fa%2F0X0000000bkF%2FOfXEFsWeXaF88kRB4Z2R2j2oda38_8B3Od1vOD1JT2M&asPdf=false2014-07-31 7:59 AM
Good grief, this is getting to be unnecessarily complicated.
The board should have 32 MB of SDRAM memory situated at 0xC0000000 in the memory map. This memory would need to be initialized (external bus, pins, control, chip) by code in system_stm32f4xx.c -> SystemInit() -> SystemInit_ExtMemCtl() Look at some FMC/FSMC example for your board STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\FMC\FMC_SDRAM STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\FMC\FMC_SRAM STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\FMC\FMC_NOR Board Support Packages STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Utilities\STM32_EVAL\STM324x9I_EVAL