2016-07-07 1:38 AM
Hi
I use EXTI for trigger ADC for stm32fRCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
/* DMA1 Channel1 Configuration ----------------------------------------------*/
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&ADC3ConvertedValue;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = 300;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
/* Enable DMA Stream Half / Transfer Complete interrupt */
//DMA_ITConfig(DMA1_Channel1, DMA_IT_TC | DMA_IT_HT, ENABLE);
/* Enable DMA1 channel1 */
DMA_Cmd(DMA1_Channel1, ENABLE);
//////////////////////////////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////////////////////////////
/* ADC1 configuration ------------------------------------------------------*/
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConv =ADC_ExternalTrigConv_Ext_IT11_TIM8_TRGO ;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 1;
ADC_Init(ADC1, &ADC_InitStructure);
//////////////////////////////////////////////////////////////////////////////////////////////////
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 1, ADC_SampleTime_1Cycles5); //c2 ==for voltage /* Regular discontinuous mode channel number configuration */
ADC_DiscModeChannelCountConfig(ADC1, 1);
/* Enable regular discontinuous mode */
ADC_DiscModeCmd(ADC1, ENABLE);
/* Enable ADC1 external trigger conversion */
ADC_ExternalTrigConvCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Enable ADC1 reset calibration register */
ADC_ResetCalibration(ADC1);
/* Check the end of ADC1 reset calibration register */
while(ADC_GetResetCalibrationStatus(ADC1));
/* Start ADC1 calibration */
ADC_StartCalibration(ADC1);
/* Check the end of ADC1 calibration */
while(ADC_GetCalibrationStatus(ADC1));
//////////////////////////////////////////////////////////////////////////////////////////////////
The below code is for configuring EXTI.
void EXTI11_Config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIOA clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);
/* Configure PA.00 pin as input floating */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Enable AFIO clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);
/* Connect EXTI0 Line to PB.11 pin */
GPIO_EXTILineConfig(GPIO_PortSourceGPIOB, GPIO_PinSource11);
/* Configure EXTI0 line */
EXTI_InitStructure.EXTI_Line = EXTI_Line11;
EXTI_InitStructure.EXTI_Mode =EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
// /* Enable and set EXTI0 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
It works. When I connect the
EXTI_Line11
to the square wave the ADC convert the analog input and put them into the ADC3ConvertedValue.
I adjust EXTI for rising and falling edge.
I want to calculate data between two rising and falling edge of the external interrupt .
But I dont know which section of the ADC3ConvertedValue is linked to the time of converting between two rising and falling edge of external interrupt?
2016-07-07 3:15 PM
What exactly do you want to measure? The maximum/peak of the triangular waveform? You might perhaps want to build an (analogue) peak detector (basically a diode and a capacitor) and measure the voltage on that, perhaps at the falling edge; you can also discharge the capacitor actively after the voltage is measured. To work out the details is upon you though.
JW