2013-11-30 9:50 AM
I am try to interrupt the STM32F100C8T6B on External interrupt on PortB.2 from Accelometer Board (the interrupt is low level while the bus is pulled up with 4.7K ohm on 3.3V) .
the case that I was polling on the low level on the Accelometer interrupt pin and it was work , when I wanted to make it using EXTI on MC , It didn't work RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB , ENABLE);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;GPIO_Init(GPIOB, &GPIO_InitStructure);GPIO_EXTILineConfig(GPIO_PortSourceGPIOB, GPIO_PinSource2);EXTI_InitTypeDef EXTI_InitStructure;EXTI_InitStructure.EXTI_Line = EXTI_Line2 ;EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;EXTI_InitStructure.EXTI_LineCmd = ENABLE;EXTI_Init(&EXTI_InitStructure);NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);NVIC_InitTypeDef NVIC_InitStructure;NVIC_InitStructure.NVIC_IRQChannel = EXTI2_IRQn;NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);and It has never entered the ISR while I am sure that the interrupt happen can anyone help me2013-11-30 2:57 PM
You need to enable the AFIO clock (SYSCLK in other STM32 series) for the EXTI peripheral block.