cancel
Showing results for 
Search instead for 
Did you mean: 

Extending program memory space - best practices Can / should QSPI flash be used to extend program memory space or is there a better method?

MColl.3
Associate II
 
1 REPLY 1

On the CM7 it is certainly one of the best combinations of speed, cost, complexity, pins, etc.

Caching hides a lot of the potential down sides.

Boards can use simpler SMT parts, lower cost PCBs.

I might use it primarily to park large graphic images.

Not particularly good for data storage or logging. For that you'd probably want to use NAND, or eMMC if you want the memory to manage itself.

One might however introspect as to whether there was a misjudgement about exactly what resources the project required at the outset. If for example a tablet SoC with large DDR3/4 memory might off better speed, resolution, or pricing.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..