2019-05-07 9:02 AM
I'm using I-CUBE-LRWAN but i have a problem with the wakeup pin (PA0): i can't "wake up" the micro from low power mode with the pin PA0 (WKUP1) of STM32L072CZY.
At PA0 I put a pull-down and a button connected to 3V3 to generate a rising edge.
I tried to insert in the code a call to HAL_PWR_EnableWakeUpPin() function with all the possible parameters (PWR_WAKEUP_PIN1 and PWR_WAKEUP_PIN2), i didn't get any results.
My main is:
int main( void )
{
/* STM32 HAL library initialization*/
HAL_Init();
/* Configure the system clock*/
SystemClock_Config();
/* Configure the debug mode*/
DBG_Init();
/* Configure the hardware*/
HW_Init();
/*Disbale Stand-by mode*/
LPM_SetOffMode(LPM_APPLI_Id , LPM_Disable );
//Configure the Lora Stack
LORA_Init( &LoRaMainCallbacks, &LoRaParamInit);
LORA_Join();
__HAL_RCC_GPIOA_CLK_ENABLE();
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
while( 1 )
{
LoRaMacProcess( );
DISABLE_IRQ( )
LPM_EnterLowPower( );
ENABLE_IRQ();
LED_Toggle(LED_BLUE);
}
}
2019-05-21 3:07 AM
Hello,
You can refer to the Standby example in the STM32Cube _FW_L0.
This example based on the wake pin.
Best Regards,
Mohamed Aymen.